RPI 2 Debugging not working.

Open source ARM Debugger

Moderator: phalanx

RPI 2 Debugging not working.

Postby arunmag » Sun May 14, 2017 5:40 am

I am using Raspberry Pi 2 B running raspbian and i have followed this tutorial https://movr0.com/2015/10/15/how-to-jta ... om-kernel/
How do i enable the JTAG and debug it?
I am on Lubuntu 17 with FT232H JTAG adapter. But i am getting this weird error.
Code: Select all
Open On-Chip Debugger 0.9.0 (2015-09-02-10:42)
Licensed under GNU GPL v2
For bug reports, read
   http://openocd.org/doc/doxygen/bugs.html
adapter speed: 2000 kHz
adapter speed: 1000 kHz
adapter_nsrst_delay: 400
none separate
Info : auto-selecting first available session transport "jtag". To override use 'transport select <transport>'.
Info : clock speed 1000 kHz
Error: JTAG scan chain interrogation failed: all ones
Error: Check JTAG interface, timings, target power, etc.
Error: Trying to use configured scan chain anyway...
Error: rpi2.dap: IR capture error; saw 0x0f not 0x01
Warn : Bypassing JTAG setup events due to errors
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
Warn : Invalid ACK 0x7 in JTAG-DP transaction
arunmag
 
Posts: 1
Joined: Sun May 14, 2017 5:38 am


Return to OpenOCD

Who is online

Users browsing this forum: No registered users and 2 guests