SparkFun Forums 

Where electronics enthusiasts find answers.

Open source ARM Debugger
By rjb_controls
#193112
Hello,

I am new to OPENOCD. I am trying program/debug TIVA TM4C1294XL board with emBitz and OPENOCD. I am getting errors as shown below. I have also pasted output with -d3 switch at the bottom. Does anyone know how to resolve this?
After a couple of tries the processor does get programmed and halts at the RESET entry but its very unreliable.

Thanks.

#######################################################
Open On-Chip Debugger 0.9.0 (2015-05-19-12:06)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 500 kHz
Info : clock speed 1965625408 kHz
Info : ICDI Firmware version: 1263
Info : tm4c1294ncpdt.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : accepting 'gdb' connection on tcp/3333
undefined debug reason 7 - target needs reset
adapter speed: 4541481 kHz
target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x000061b4 msp: 0x20010a40
adapter speed: 4541481 kHz
target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x000061b4 msp: 0x20010a40
target state: halted
target halted due to breakpoint, current mode: Thread
xPSR: 0x61000000 pc: 0x20000042 msp: 0x20010a40
adapter speed: 4541481 kHz
target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x00000ad8 msp: 0x20000200
adapter speed: 4541481 kHz
Error: memory write failed: 0x7
Error: memory write failed: 0x7
Error: memory read failed: 0x7
Error: jtag status contains invalid mode value - communication failure
TARGET: tm4c1294ncpdt.cpu - Not halted
in procedure 'reset'
in procedure 'ocd_bouncer'


adapter speed: 4541481 kHz
target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x00000ad8 msp: 0x20000200