- Mon Jul 18, 2016 12:13 am
#190680
Hey all,
I'm trying to burn the Arduino Zero bootloader with the Atmel-ICE and the OpenOCD command.
When I do it from the Arduino IDE everything is OK and I can burn it in one click. Later I tried to execute the same command from the "command line" (windows cmd), but it didn't work - it is stuck after "Info : at91samd21g18.cpu: hardware has 4 breakpoints, 2 watchpoints".
Any idea?
Thanks!
I'm trying to burn the Arduino Zero bootloader with the Atmel-ICE and the OpenOCD command.
When I do it from the Arduino IDE everything is OK and I can burn it in one click. Later I tried to execute the same command from the "command line" (windows cmd), but it didn't work - it is stuck after "Info : at91samd21g18.cpu: hardware has 4 breakpoints, 2 watchpoints".
Any idea?
Thanks!
Code: Select all
openocd.exe -d2 -s "C:\Users\me\AppData\Local\Arduino15\packages\arduino\tools\openocd\0.9.0-arduino/share/openocd/scripts/" -f "C:\Users\me\AppData\Local\Arduino15\packages\arduino\hardware\samd\1.6.2/variants/arduino_zero/openocd_scripts/arduino_zero.cfg" -c telnet_port disabled; init; halt; at91samd bootloader 0; program {{"C:\Users\me\AppData\Local\Arduino15\packages\arduino\hardware\samd\1.6.2/bootloaders/zero/samd21_sam_ba.bin"}} verify reset; shutdown
Open On-Chip Debugger 0.9.0-gd4b7679 (2015-06-10-22:24)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
debug_level: 2
cygwin warning:
MS-DOS style path detected: C:\Users\me\AppData\Local\Arduino15\packag
es\arduino\hardware\samd\1.6.2/variants/arduino_zero/openocd_scripts/arduino_zer
o.cfg
Preferred POSIX equivalent is: /cygdrive/c/Users/me/AppData/Local/Ardu
ino15/packages/arduino/hardware/samd/1.6.2/variants/arduino_zero/openocd_scripts
/arduino_zero.cfg
CYGWIN environment variable option "nodosfilewarning" turns off this warning.
Consult the user's guide for more details about POSIX paths:
http://cygwin.com/cygwin-ug-net/using.h ... -pathnames
Info : only one transport option; autoselect 'swd'
adapter speed: 500 kHz
adapter_nsrst_delay: 100
cortex_m reset_config sysresetreq
4444
Info : CMSIS-DAP: SWD Supported
Info : CMSIS-DAP: JTAG Supported
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : CMSIS-DAP: FW Version = 01.1C.0067
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 1 TDO = 1 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 500 kHz
Info : SWD IDCODE 0x0bc11477
Info : at91samd21g18.cpu: hardware has 4 breakpoints, 2 watchpoints