- Wed May 25, 2016 10:05 am
#189957
Hey,
I have an ARC uC SoC I want to debug.
The Toolchain I use is the GNU ARC compiler from the https://www.embarc.org/ project.
This is using OpenOCD to make a connetion to the Target (ARC EM4 Core, custom board).
My digilent USB-JTAG cable is recognized by Win7 as an ftdi device with vid 0403, pid 6010.
I know the cable is working because it works with another project under SynopsisMetawareDebugger.
My problem is that I get the following error message when trying to start the debug session:
Can anyone help me out with this, or at least give a hint please?
thanks a lot!
xaver_aed
I have an ARC uC SoC I want to debug.
The Toolchain I use is the GNU ARC compiler from the https://www.embarc.org/ project.
This is using OpenOCD to make a connetion to the Target (ARC EM4 Core, custom board).
My digilent USB-JTAG cable is recognized by Win7 as an ftdi device with vid 0403, pid 6010.
I know the cable is working because it works with another project under SynopsisMetawareDebugger.
My problem is that I get the following error message when trying to start the debug session:
Open On-Chip Debugger 0.9.0-dev-g8a252b3 (2015-06-08-13:44)I haven't any clue how to fix that...
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
debug_level: 0
adapter speed: 10000 kHz
Error: unable to open ftdi device: device not found
Error: ListDevices: 2
Error: 0: "Dual RS232 A"
Error: 1: "Dual RS232 B"
Runtime Error: C:\arc_gnu\share\openocd\scripts\board\snps_em_sk_v2.cfg:48:
in procedure 'script'
at file "embedded:startup.tcl", line 58
in procedure 'init' called at file "C:\arc_gnu\share\openocd\scripts\board\snps_em_sk_v2.cfg", line 48
Can anyone help me out with this, or at least give a hint please?
thanks a lot!
xaver_aed