- Thu Sep 14, 2006 5:41 am
#18869
Hi all,
I try to find a way to debug my application on flash. I'm very not an expert with all the dgb stuff. I can get some part of the chain working but i cannot get the debug (breakpoint , single step etc) working.
Can somebody tell me or give me the link to get this setup working.
AT91sam7S256
Debug in flash
openocd rev93
eclipse with all the cdt plugins installed.
I have follow the tutorial from lynch but this one is for ram debug only i think.
What i need in my cfg file for openocd
what is the gdb command i have to send from eclipse
What is the debug information i have to have in my makefile (dwarf-2 ?)
OPT = 0
what else ?
wig.cfg
I try to find a way to debug my application on flash. I'm very not an expert with all the dgb stuff. I can get some part of the chain working but i cannot get the debug (breakpoint , single step etc) working.
Can somebody tell me or give me the link to get this setup working.
AT91sam7S256
Debug in flash
openocd rev93
eclipse with all the cdt plugins installed.
I have follow the tutorial from lynch but this one is for ram debug only i think.
What i need in my cfg file for openocd
what is the gdb command i have to send from eclipse
What is the debug information i have to have in my makefile (dwarf-2 ?)
OPT = 0
what else ?
wig.cfg
Code: Select all
eclipse command
# OPENOCD "Batch"-Programming
# for Atmel SAM7 ARM7TDMI
#
# Using a Wiggler-Type JTAG-Interface
# Adapted by Martin Thomas (www.siwawi.arubi.uni-kl.de/avr_projects)
# Based on information from Dominic Rath - Thank you!
#daemon configuration
telnet_port 4444
gdb_port 3333
#interface
interface parport
parport_cable wiggler
parport_port 0x378
jtag_speed 0
#use combined on interfaces or targets that can't set TRST/SRST separately
## mthomas: used this for Atmel SAM7S64-EK
reset_config srst_only
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 4 0x1 0xf 0xe
#target configuration
daemon_startup reset
#target
#target arm7tdmi
target arm7tdmi little run_and_init 0 arm7tdmi_r4
run_and_halt_time 0 30
working_area 0 0x00100000 0x40000 nobackup
flash bank at91sam7 0 0 0 0 0
# mthomas AT91SAM7
Code: Select all
Jonathantarget remote localhost:3333
monitor soft_reset_halt
monitor reg pc 0x00000000
monitor ARM7_9 force_hw_bkpts enable
break main
load
continue