- Tue Nov 18, 2014 12:31 pm
#176985
Ok folks I'm a bit at a loss here. Basic environment:
Ubuntu 14.04LTS
OpenOCD 0.8.0 built and installed from source (removed the debian openocd package)
Nucleo STM32L03
STM32L0-Discovery (e-paper discovery board)
I've flashed the Nucleo to the latest firmware using a windows machine and the STMicro tool.
I've used openocd before on my ST discovery boards it was fine, these boards use 'STLink V2.1' which changes two things, one is that they support 'mBed' (which means they are now composite USB devices exporting a storage device, a CDC (serial port), and their debugging port), the other is that the STLink protocol has been updated to 2.1-1 (sort of a 2.1.1 I guess).
Anyway, my openocd.cfg file has simply this in it:
I'm trying to figure out how to get this thing going, does anyone else have this board combo running?
--Chuck
Ubuntu 14.04LTS
OpenOCD 0.8.0 built and installed from source (removed the debian openocd package)
Nucleo STM32L03
STM32L0-Discovery (e-paper discovery board)
I've flashed the Nucleo to the latest firmware using a windows machine and the STMicro tool.
I've used openocd before on my ST discovery boards it was fine, these boards use 'STLink V2.1' which changes two things, one is that they support 'mBed' (which means they are now composite USB devices exporting a storage device, a CDC (serial port), and their debugging port), the other is that the STLink protocol has been updated to 2.1-1 (sort of a 2.1.1 I guess).
Anyway, my openocd.cfg file has simply this in it:
Code: Select all
My /etc/udev has the appropriate rule set (for the updated VID/PID of these new boards) :
source [find board/st_nucleo_f030r8.cfg]
Code: Select all
When I start OpenOCD it responds thusly:# STlink
ATTRS{idVendor}=="0483", ATTRS{idProduct}=="374b", MODE="666", GROUP="plugdev"
Code: Select all
It seems like it is trying to use the JTAG api but these chips only offer the SWD api. (one of the conceits for the low power ness of the L0 version according to the FE at a recent seminar)Open On-Chip Debugger 0.8.0 (2014-11-16-21:54)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_deassert_srst
Info : This adapter doesn't support configurable speed
Info : STLINK v2 JTAG v21 API v2 SWIM v5 VID 0x0483 PID 0x374B
Info : using stlink api v2
Info : Target voltage: 3.218935
Error: hl_interface_init_target: target not found: idcode: 0x0bc11477
in procedure 'transport'
in procedure 'init'
I'm trying to figure out how to get this thing going, does anyone else have this board combo running?
--Chuck