- Mon Aug 25, 2014 10:56 am
#174127
Hello everyone,
I'm Newbie to the JTAG related stuff, and i'm here to ask some senior's help.
I want to learn about how to control a chip using JTAG, so I bought myself a JTAG adapter, BUS BLASTER v4, to be precise, and I found among my old stuff a platform on which experiment.
I found an old firewall which has as main CPU a Conexant cx82100.
I verified through the datasheet, it have pins dedicated to JTAG function, and I therefore I assumed it could be a feasible target.
Launching OpenOCD, it spawns something like this:
Due to my lack of knowledge I have difficulties on the interpretation of this data.
I noticed however that TDO is is doing some activities:
Can someone help me on this?
Thank you
Regards.
AC
I'm Newbie to the JTAG related stuff, and i'm here to ask some senior's help.
I want to learn about how to control a chip using JTAG, so I bought myself a JTAG adapter, BUS BLASTER v4, to be precise, and I found among my old stuff a platform on which experiment.
I found an old firewall which has as main CPU a Conexant cx82100.
I verified through the datasheet, it have pins dedicated to JTAG function, and I therefore I assumed it could be a feasible target.
Launching OpenOCD, it spawns something like this:
Code: Select all
It seems to me there's something wrong: for example I expected to see something different from 0x00000000 in the IdCode field.root@c2:~# openocd
Open On-Chip Debugger 0.8.0 (2014-08-18-16:12)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'jtag'
adapter speed: 500 kHz
Info : clock speed 500 kHz
Warn : There are no enabled taps. AUTO PROBING MIGHT NOT WORK!!
Warn : AUTO auto0.tap - use "jtag newtap auto0 tap -expected-id 0x00000000 ..."
Warn : AUTO auto1.tap - use "jtag newtap auto1 tap -expected-id 0x00000000 ..."
Warn : AUTO auto0.tap - use "... -irlen 2"
Error: auto0.tap: IR capture error; saw 0x0003 not 0x0001
Warn : Bypassing JTAG setup events due to errors
Warn : gdb services need one or more targets defined
Info : accepting 'telnet' connection from 4444
Info : TAP auto0.tap does not have IDCODE
Info : TAP auto1.tap does not have IDCODE
Error: auto0.tap: IR capture error; saw 0x0003 not 0x0001
Warn : Bypassing JTAG setup events due to errors
TapName Enabled IdCode Expected IrLen IrCap IrMask
-- ------------------- -------- ---------- ---------- ----- ----- ------
0 auto0.tap Y 0x00000000 0x00000000 2 0x01 0x03
1 auto1.tap Y 0x00000000 0x00000000 0 0x00 0x00
Due to my lack of knowledge I have difficulties on the interpretation of this data.
I noticed however that TDO is is doing some activities:
Can someone help me on this?
Thank you
Regards.
AC