- Thu Jan 30, 2014 9:34 pm
#167884
I am having some difficulties in connecting the C232HM-EDHSL-0. I have created the (temporary) .cfg:
It is not my belief that the drivers are to be suspect as the device name is successfully retrieved, and other FTDI devices do function as desired. In addition, this device does function elsewhere.
It is my hope that someone has some light to shed upon this. Any assistance would be greatly appreciated...
interface ft2232However, when this is run, the result is:
ft2232_device_desc "C232HM-EDHSL-0"
ft2232_layout usbjtag
ft2232_vid_pid 0x0403 0x6010
adapter_khz 1000
Open On-Chip Debugger 0.8.0-dev-00301-g416e79e (2014-01-22-20:53)It does appear that the program is stating that "C232HM-EDHSL-0" does not match "C232HM-EDHSL-0".
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'jtag'
adapter speed: 1000 kHz
Warn : Unable to open FTDI Device tried: 'C232HM-EDHSL-0' and 'C232HM-EDHSL-0 A'
Error: unable to open ftdi device: device not found
Error: ListDevices: 1
Error: : "C232HM-EDHSL-0"
in procedure 'init'
It is not my belief that the drivers are to be suspect as the device name is successfully retrieved, and other FTDI devices do function as desired. In addition, this device does function elsewhere.
It is my hope that someone has some light to shed upon this. Any assistance would be greatly appreciated...