- Fri Jun 16, 2006 11:56 am
#14619
Hi,
I am trying to use OpenOcd (Rev. 65) with a board with an AT91RM9200.
I am using an original Wiggler connected to the board, but I have also
tested with some clones.
Openocd is running in Ubuntu 6.06 and the command "poll"
reports that the target is running.
The command "wait_halt" ends with timeout.
If I use the same board and wiggler connected to a Windows box,
OCD Commander (from Macraigor) manages to halt the target at start-up
(after some time), but if I reset the target,
OCD commander could not also put the target in debug mode.
I have to exit from OCD commander and start it again.
I have tried lower speeds and the results are the same.
Follows my configuration file for OpenOcd:
The board seems to be working OK
Regards,
Claudio
I am trying to use OpenOcd (Rev. 65) with a board with an AT91RM9200.
I am using an original Wiggler connected to the board, but I have also
tested with some clones.
Openocd is running in Ubuntu 6.06 and the command "poll"
reports that the target is running.
The command "wait_halt" ends with timeout.
If I use the same board and wiggler connected to a Windows box,
OCD Commander (from Macraigor) manages to halt the target at start-up
(after some time), but if I reset the target,
OCD commander could not also put the target in debug mode.
I have to exit from OCD commander and start it again.
I have tried lower speeds and the results are the same.
Follows my configuration file for OpenOcd:
Code: Select all
Any ideas what could be wrong ?#daemon configuration
telnet_port 4444
gdb_port 8888
#interface
interface parport
parport_port 0x378
parport_cable wiggler
jtag_speed 3
#use combined on interfaces or targets that can't set TRST/SRST separately
reset_config trst_and_srst
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 4 0x1 0xf 0xe
#target configuration
daemon_startup reset
#target <type> <startup mode>
target arm9tdmi little reset_halt 0 arm920t
run_and_halt_time 0 30
The board seems to be working OK
Regards,
Claudio