SparkFun Forums 

Where electronics enthusiasts find answers.

Have questions about SparkFun's ALC PCB design services? Post them here!
User avatar
By Kcoolz
#228677
HI,

We are working on a rover and wanted to know if it would be possible to make a board to make it easier to mount and have less wires. I'm new to this and not sure how the a la carte design works. All we need is an ESP32 with 2 RTK2.

Here is a screenshot of how our wiring looks between them. If someone is able to guide me in the right direction that would be great!

Image
User avatar
By sparky
#228710
It's not possible on ALC at the moment because we've set the limit of one ZED per design. But that's because I assumed no one would ever want two ZEDs on a single board. Silly assumption on my part!

What are you building? It looks like one ZED is providing the correction data to the 2nd ZED. That makes sense for a moving baseline application but I've only seen those needed in aerospace applications.

If I were prototyping two ZEDs, I would use Qwiic and daisy chain them on any of our ESP32 boards that has a Qwiic connector. You'd need to change the I2C address of one of the modules using u-center (via USB) or over I2C but it works fine.

Once I understand your application a bit more we can easily configure the ALC block to allow for multiple on one board.
User avatar
By Kcoolz
#228722
Yeah we are creating a autonomous rover which we use a moving baseline to calculate yaw. Since our base is metal we it made more sense to use 2 GPS's without any compasses.

The ESP is getting corrections from our stationary base, feeding it to the first ZED. And then that ZED is feeding its moving corrections to the other one.

We were mostly interested in ALC just to combine them into 1 board which would reduce wires needed and it would have a smaller form factor.
User avatar
By sparky
#228726
Ah, that makes more sense. What is the ESP sending via UART2 to the ZED1? That's customarily RTCM (but can be anything really) and not what I would expect coming from an ESP.
 Topic permissions

You can post new topics in this forum
You can reply to topics in this forum
You cannot edit your posts in this forum
You cannot delete your posts in this forum
You cannot post attachments in this forum

long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]