SparkFun Forums 

Where electronics enthusiasts find answers.

Hardware or product specific questions are best asked here.
User avatar
By MatMor90
#229036
Hello everybody,
Just one quick question about the Artemis thing plus:
I plan to connect it to an F9P-RTK 2 with a Bluetooth mate gold connected to its UART, and an oled lcd. I was wondering if the Artemis thing plus board would be able to power all of the above via the i2c bus.

I saw that the Redboard Artemis has a max of 600 mA current output, but no such specification is provided fo the Thing Plus.

Can you tell me the max current that the Thing Plus is capable to provide?

Thanks
User avatar
By TS-Russell
#229061
It should also be 600mA...looking at the two perihperals, you should have plenty of power for those 2 :-D

Mate Gold: ~25mA
F9p: Current: 68mA - 130mA (varies with constellations and tracking state)
 Topic permissions

You can post new topics in this forum
You can reply to topics in this forum
You cannot edit your posts in this forum
You cannot delete your posts in this forum
You cannot post attachments in this forum