SparkFun Forums 

Where electronics enthusiasts find answers.

Hardware or product specific questions are best asked here.
User avatar
By joe5939
#225704
Is it possible to adjust the LiPo charging current on the MCP73831 with software to make it safe for a battery smaller than 450mAh? I see there is a 2.2kOhm R4 tied to pin 5. I really don't want to try to replace that tiny little component with a 10kOhm unless that is the only way.


"Please make sure your battery capacity is at least 450mAh (0.45Ah); bad things will happen if you try to charge our smallest batteries at 450mA. "
User avatar
By TS-Chris
#225705
Unfortunately that's the only way to change the charge current, swapping the 2.2K resistor for a 10K resistor would change the charge current to 100mA though.
16832-SparkFun_OpenLog_Artemis-03.jpg
You do not have the required permissions to view the files attached to this post.