- Wed Nov 04, 2020 1:55 am
#220407
I'm having trouble using the OLA Dev-16832 to read data from the SHTC3 board when it is connected to the 8 channel qwiic max breakout board. It will read it ONLY when plugged directly into the OLA qwiic port. I read that its address is 0x70 which seems to be the same as the mux board, but don't know if that's a problem or not, since the max board should give it another port number, but...? I'm trying to read data from two MPR0025MPA MicroPressure sensors and the SHTC3 at the same time, but it just will not work. Tried different cables, different ports on the Mux board. Interestingly, some ports make the OLA give me the error "Known I2C address but device failed identification at address 0x70" while others don't recognize the SHTC3 is even there. What am I missing?
Thanks
Thanks