SparkFun Forums 

Where electronics enthusiasts find answers.

Hardware or product specific questions are best asked here.
User avatar
By marco.bernardini
#231962
Hi all,
this is my first post on this forum.
I’ve a question regarding the “Artemis Global Tracker” (https://www.sparkfun.com/products/18712).
In the past I used Iridium Modem with two kind of protocols: connection mode (Rudics) and message based.
If I understood correctly the Artemis Global Tracker is configured to work with the RockBLOCK provider and it’s message based. I need to send a block of data that can be 8Kbytes.Do you know if it can be used with other provider that support connected mode?
With connected mode I mean that the Modem make a call to another modem to establish a TCP connection.
User avatar
By PaulZC
#231966
Hello @marco.bernardini,

The Artemis Global Tracker uses the Iridium 9603N modem which is only capable of Short Burst Data (SBD) transfers. It is not like the other Iridium modems which support connected mode. You would need to divide your 8K of data into 340 byte chunks and transfer them one at a time.

Best wishes,
Paul
User avatar
By PaulZC
#231967
Also:

If you want to transfer all 8K bytes to another modem, you are actually limited to 270 bytes per message. The limits for SBD transfers are 270 bytes received, 340 bytes transmitted.

Best wishes,
Paul
#239531
I'm getting conflicting advice on whether the Artemis on the AGT could be used for all of the IoT processing
Some are saying it can't handle external IO, while others are saying an external Nano could process the
IO and/or modbus RTU vis rs485 comms

Ideally the resultant system would have the capability of:
2 or 3 analog IN
2 or 3 Digital IN
1 (high speed) Digital counter input for measuring period / frequency
1 or 2 Digital OUT
If not too hard: RS485 for retrieving device data via Modbus RTU
If the AGT WRL-18712 can handle a chunk of that and maybe use a Uno or Nano for additional IO

Could the AGT use an Arduino.cc MKR rs485 shield ?
I assume that the native serial channels are already busy with GPS and Sat

Regards...
 Topic permissions

You can post new topics in this forum
You can reply to topics in this forum
You cannot edit your posts in this forum
You cannot delete your posts in this forum
You cannot post attachments in this forum

long long title how many chars? lets see 123 ok more? yes 60

We have created lots of YouTube videos just so you can achieve [...]

Another post test yes yes yes or no, maybe ni? :-/

The best flat phpBB theme around. Period. Fine craftmanship and [...]

Do you need a super MOD? Well here it is. chew on this

All you need is right here. Content tag, SEO, listing, Pizza and spaghetti [...]

Lasagna on me this time ok? I got plenty of cash

this should be fantastic. but what about links,images, bbcodes etc etc? [...]