SparkFun Forums 

Where electronics enthusiasts find answers.

Hardware or product specific questions are best asked here.
By Ribinn
#232836
Hi,
I have understood that the onboard IMU of the Artemis Module could deliver and record directly the Euler angles from quaternion angles. I just tried to upload the IMU DMP Quat6 but the Arduino OLE tells me there is a trouble with a declaration (see attached picture).
So is it possible to get a help on that and on the way to record Euler angles. I must say that I still need to record GNSS data (10 Hz for the moment as discussed in an other topic).

Regards
Christian
You do not have the required permissions to view the files attached to this post.
User avatar
By PaulZC
#232843
Hello Christian,

You have the Pro nRF52840 Mini board selected. You need to select the SparkFun Apollo3 \ RedBoard Artemis ATP.

That code example was written for version 2.1.0 of Apollo3, but it should work perfectly with v2.2.1 (the latest version).

Best wishes,
Paul
You do not have the required permissions to view the files attached to this post.
By Ribinn
#232852
Hi, Paul
I make slow but real progress as I am OK to compil the examples quat9 or 6.
But it is required to edit the ICM_20948_C.h to enable the use of the DMP.
I have found the file and the line but I am not easy on the process after that : where to change and copy the new file ?

Christian
User avatar
By PaulZC
#232883
Hello Christian,

It sounds as if you are quite new to changing and compiling Arduino code? There are many easier examples you could work through to build your experience. Modifying and re-building the full OpenLog Artemis code is a large and quite complex project.

You can find more information about the DMP here:

https://github.com/sparkfun/SparkFun_IC ... ain/DMP.md

But, to answer your question, you need to modify and save (overwrite) the ICM_20948_C.h. Do not change its name. Do not change its location. The compiler will use the updated file when you re-compile the code.

Best wishes,
Paul
By Ribinn
#233036
Hi Paul,
I tried to use Example6 and 7 quat9 and quat6 orientation after trying to modify the 20948_C.h file.
But I found that your proposed procedure to modify this file was not obvious for me as it is required to ask for a pull request in place of saving the change ... I tried that till the point in the attached image ...
Assuming that the modified files could have arrived somewhere in my directory (???), I tried to upload the Example7 and 6.
I got an appearance of upload success but with no initialization of the Artemis according to the com7 view (see the second image)

Please don't forget that my need is to get orientation angles together with GPS data ???

Regards
Christian
You do not have the required permissions to view the files attached to this post.
User avatar
By PaulZC
#233039
Hello Christian,

Please use the OLA BETA binary. Open the main menu, then the IMU menu. There is an option to enable the DMP. Once enabled, you will be able to log Quat6 or Quat9 data simultaneously with your GNSS data.

Best wishes,
Paul
By Ribinn
#233052
Hi ,Paul
Thank you for your answer.
The good news is that simultaneous attitude and GNSS data recording is possible

But, for the moment, sorry as I have not found something with name "OLA BETA binary"

Assuming that enabling the DMP option could also be done with the Terminal connection, I tried to configure it in accordance with the attached image.
Then, I uploaded the "Example7 ... Quat6..." but it also ended with incorrect initialization !

Christian
You do not have the required permissions to view the files attached to this post.
User avatar
By PaulZC
#233055
Hello Christian,

The "OLA BETA binary" is the Beta firmware I created for you to let you log the GNSS data at 25Hz:

https://github.com/sparkfun/OpenLog_Art ... 3_BETA.bin

https://en.wikipedia.org/wiki/Software_ ... cycle#Beta

The IMU menu is the same as for the standard OpenLog Artemis. Using the Beta firmware, you will be able to log the GNSS data and the IMU quaternion data at 25Hz.

You can not use Examples 6 and 7 from the ICM20948 library directly on OpenLog Artemis. Extra code is required to configure the board correctly (enable power for the IMU, enable the POCI pull-up). If you want to experiment, please use the dedicated "IMU_DMP_Quat6" and "IMU_DMP_Quat9" examples from here:

https://github.com/sparkfun/OpenLog_Art ... 20Sketches

Best wishes,
Paul
By Ribinn
#233061
Thank you so much Paul,
In fact the Beta version works perfectly and gives the quaternion Q6 data. (see attached)

However, I see that It gives Q data but does not give Euler angles.
Those angles seems to be normal output of "Example7_DMP_Quat6_EulerAngles firmware" (see attached).

So my question is about the possibility and the difficulty to add this conversion in your Beta version ?

Regards

Christian
You do not have the required permissions to view the files attached to this post.
User avatar
By PaulZC
#233078
Hello Christian,

I regret you will need to convert the quaternions to Euler angles manually, on the logged data. You will be able to do it in a spreadsheet like Excel. The logged data is in Comma Separated Value format which Excel will understand. Or you could use the Python CSV library.

Please be aware:

https://github.com/sparkfun/SparkFun_IC ... /issues/74

https://github.com/sparkfun/SparkFun_IC ... /issues/77

https://github.com/sparkfun/SparkFun_IC ... -863134578

Good luck with your project!

Best wishes,
Paul
By Ribinn
#233085
OK Paul for a post conversion.

Another solution would be to change my configuration toward a "Sparkfun 9DoF ImU" (20948), which seems to produce Euler angles, connected with the NEO-M9N to a basic Qwiic OpenLog.
But I think that this would require firmware works ...

Christian
 Topic permissions

You can post new topics in this forum
You can reply to topics in this forum
You cannot edit your posts in this forum
You cannot delete your posts in this forum
You cannot post attachments in this forum