- Sat Feb 03, 2024 3:03 am
#246885
Hi all,
I am planning a project with the Artemis ATP and Super Wav Trigger. While the Super Wav Trigger will have its own step-down converter and is isolated from the 3.3V I2C/Qwiic line, I plan to use the Artemis ATP to power everything else, which would be:
1x SSD1306 OLED Display (roughly 25mA) via I2C/Qwiic
1x SX1509 GPIO Extender (monitoring 16 active low switches) via I2C/Qwiic
1x SX1509 GPIO Extender via I2C/Qwiic driving 12 white LEDs either in current source mode (the 8 mA per pin are plenty in terms of brightness for me, so that would be roughly 100mA via the I2C connection) or current sink mode (which the manual says is more efficient) with connecting VCC1 and VCC2 to the 3.3V of Artemis ATP and using an appropriate resistor per LED to keep current in 5 mA range per LED.
1x CD74HC4067 with 12x 10k pots connected to 3.3V
Two more pots and an indicator LED directly connected to the GPIO pins of Artemis ATP.
I've read that the Artemis can set the current on a per pin basis from 2 to 12mA (so this would be the maximum per pin?). But I haven't found any infos on what is the maximum current the Artemis ATP can provide to peripherals. What can I draw maximum from the 3.3V pin safely (is it LM317-based, so 1.5A?)? What are the Artemis ATP GPIOs capabilities to sink current? Is there anything I should be aware of ? Another question concerning the SX1509: In order to daisy chain them, I can just connect one board to the next one via their input headers, right?
Thank you!
I am planning a project with the Artemis ATP and Super Wav Trigger. While the Super Wav Trigger will have its own step-down converter and is isolated from the 3.3V I2C/Qwiic line, I plan to use the Artemis ATP to power everything else, which would be:
1x SSD1306 OLED Display (roughly 25mA) via I2C/Qwiic
1x SX1509 GPIO Extender (monitoring 16 active low switches) via I2C/Qwiic
1x SX1509 GPIO Extender via I2C/Qwiic driving 12 white LEDs either in current source mode (the 8 mA per pin are plenty in terms of brightness for me, so that would be roughly 100mA via the I2C connection) or current sink mode (which the manual says is more efficient) with connecting VCC1 and VCC2 to the 3.3V of Artemis ATP and using an appropriate resistor per LED to keep current in 5 mA range per LED.
1x CD74HC4067 with 12x 10k pots connected to 3.3V
Two more pots and an indicator LED directly connected to the GPIO pins of Artemis ATP.
I've read that the Artemis can set the current on a per pin basis from 2 to 12mA (so this would be the maximum per pin?). But I haven't found any infos on what is the maximum current the Artemis ATP can provide to peripherals. What can I draw maximum from the 3.3V pin safely (is it LM317-based, so 1.5A?)? What are the Artemis ATP GPIOs capabilities to sink current? Is there anything I should be aware of ? Another question concerning the SX1509: In order to daisy chain them, I can just connect one board to the next one via their input headers, right?
Thank you!