Hi Paul, Thank you for your reply! This is
very helpful, and perhaps a little different than what I thought.
I installed the Artemis Uploader App:
https://github.com/sparkfun/Artemis-Firmware-Upload-GUI
I didn't have a proper Artemis board connected, so of course if failed, but "Update Bootloader" seems to automatically create "artemis_svl.bin" and would have flashed it for me? Do you agree this the correct procedure?
Artemis Bootloader Upload
Baud: 115200
File: C:\Users\mej\AppData\Local\Temp\_MEI434882\resource\artemis_svl.bin
Port: \\.\COM14
Header Size = 0x80
original app_size 0x328c ( 12940 )
load_address 0xc000 ( 49152 )
app_size 0x328c ( 12940 )
w0 = 0xcb00330c
Security Value 0x10
w2 = 0x10008080
addrWord = 0xc000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0xc703da31
Writing to file C:\Users\mej\AppData\Local\Temp_OTA_blob.bin
testing: C:\Users\mej\AppData\Local\Temp_OTA_blob.bin
Header Size = 0x60
app_size 0x330c ( 13068 )
Writing to file C:\Users\mej\AppData\Local\Temp_Wired_OTA_blob.bin
Image from 0x0 to 0x330c will be loaded at 0x20000
Connecting over serial port \\.\COM14...
Baud rate: 115200
Sending Hello.
No response for command 0x00000000
Failed to respond
Fail
Sending Hello.
No response for command 0x00000000
Failed to respond
Fail
Sending Hello.
No response for command 0x00000000
Failed to respond
Fail
Tries = 3
Upload failed
Complete.
I bought the Artemis RedBoard, but it looks like the "RedBoard Artemis ATP" (
https://www.sparkfun.com/products/15442 ) already has the JTAG broken out. Do you think I could use the ATP version to simulate what I am trying to do (pretend the Artemis on the ATP is my "recreated" Artemis on my mainboard) and reflash the bootloader?
Also, I'm still a little fuzzy about the exact purpose of the bootloader. Everything I read regarding this Sparkfun bootloader seems to refer to the resulting baud rate. I don't need to flash my app firmware over USB. If possible, I would be satisfied to break out JTAG and flash it that way.
I'd be happy to just have everything work, but in the spirit of understanding better... What does the Sparkfun Bootloader actually allow one to do? Flash via USB? Faster Flashing? Something more??
Thanks again for your reply!