- Sat Feb 25, 2023 1:20 pm
#239300
Hello All -
Does anyone know what registers to set to enable the BLE functions in the Artemis Module without the need to add an external 32 kHz crystal? I can load and run code without the crystal, but BLE only works when I add the crystal. This has supposedly been solved (post #224144), but no details were given. I've played around with the obvious register (BLEIF->CLKCFG_b.CLK32KEN), but setting it to zero just results in the code hanging. I'm clearly missing something.
Does anyone know what registers to set to enable the BLE functions in the Artemis Module without the need to add an external 32 kHz crystal? I can load and run code without the crystal, but BLE only works when I add the crystal. This has supposedly been solved (post #224144), but no details were given. I've played around with the obvious register (BLEIF->CLKCFG_b.CLK32KEN), but setting it to zero just results in the code hanging. I'm clearly missing something.