SparkFun Forums 

Where electronics enthusiasts find answers.

Tips, tricks, & best best practices using Artemis with your board designs.
User avatar
By the_commissioner
#238586
Hello,

I am looking for a Dimensional drawing of the Sparkfun Redboard Artemis ATP.

Specifically, I would like to know where the 4 mounting holes are at (see image attached).

If seems the holes are for an M3 screw. It would be helpful to list the dimensional drawings on the product page on sparkfun along with the size of the mounting holes. I see them for other products but not for this one.

The hardware files are on github, but I do not have the eagle program to be able to view them and take measurements.

Thank you,
-manuel
You do not have the required permissions to view the files attached to this post.
By paulvha
#238592
You can always try to free BRD viewer online e.g. https://www.altium.com/viewer/ to upload a BRD online.
A bit more information might help you. Looking at your picture.
The external size of the ATP is 590mm x 1018mm
The holes are 3.3mm (thus M3)
The center of the holes you indicated are all 5.0mm from the long sides.
Hole_1: The center hole top left: is 92 mm from the right hand
Hole_2: The center hole top right: 15 mm from the right hand
Hole_3: The center hole bottom left: is 965mm from the right hand
Hole_4: The center hole bottom right: is 14mm from the right hand

hope that helps.
User avatar
By PaulZC
#238603
Hi,

I think the Altium Viewer must have confused inches and mm in some way? Or perhaps cm and mm? Maybe there is a setting that can be changed.

I've attached the dimensions from Eagle. The units are inches. I hope this helps.

Best wishes,
Paul
ATP_Dimensions.jpg
You do not have the required permissions to view the files attached to this post.
 Topic permissions

You can post new topics in this forum
You can reply to topics in this forum
You cannot edit your posts in this forum
You cannot delete your posts in this forum
You cannot post attachments in this forum