- Sun Mar 28, 2021 6:45 am
#224449
Hi,
I am planning to use the SparkFun MicroMod Artemis Processor for a custom project and I have the following questions.
The project will need a multi slave scheme: up to 4 SPIs (CLK and MISO) and up to 8 CS shared across the SPIs. As I have seen the features, I am bit confused. It mentions that the Artemis chip has 6 SPI's but this is not possible on MicroMod Artemis. Can you please clarify if I reconfigure the ports differently from those you have set-up in that module so I can meet the requirements of the project?
Moreover, I will also need one extra SPI for the SD card. Is the SDIO protocol possible?
Thanks
I am planning to use the SparkFun MicroMod Artemis Processor for a custom project and I have the following questions.
The project will need a multi slave scheme: up to 4 SPIs (CLK and MISO) and up to 8 CS shared across the SPIs. As I have seen the features, I am bit confused. It mentions that the Artemis chip has 6 SPI's but this is not possible on MicroMod Artemis. Can you please clarify if I reconfigure the ports differently from those you have set-up in that module so I can meet the requirements of the project?
Moreover, I will also need one extra SPI for the SD card. Is the SDIO protocol possible?
Thanks