- Thu Dec 13, 2007 11:02 am
#39557
I'm currently running a Lassen IQ at 3.3V regulated down from a single LiPoly cell (4.2V max). I'm looking into using EM406 -- it's almost the same size, but spec says it requires 4.5 - 6.5 volts DC input.
Any idea if I can run it lower? I would assume that this module has an on-board power regulator that's creating 3.3V onboard -- does anyone know if 3.5 volts or so will work? I'd hate to have to bump up my Voltage just to have it regulated back down.
Thanks, Greg
Any idea if I can run it lower? I would assume that this module has an on-board power regulator that's creating 3.3V onboard -- does anyone know if 3.5 volts or so will work? I'd hate to have to bump up my Voltage just to have it regulated back down.
Thanks, Greg
RF Beacons and GPS Telemetry Transmitters
http://www.bigredbee.com
http://www.bigredbee.com