- Wed Oct 10, 2007 8:54 am
#36239
Hi
I'm trying to open an UDP socket via python script, but when I send the command AT#SKTOP, I receive the message NO CARRIER from the module.
I know that the problem isn't the configuration because I can open the socket via AT commands. Does any one have any idea of how can I fix it?
I'm using the 7.02.403 firmware version.
If there is any other relevant information that you need to think about the solution, just ask. But remember that I can connect via AT commands.
Thanks!!
I'm trying to open an UDP socket via python script, but when I send the command AT#SKTOP, I receive the message NO CARRIER from the module.
I know that the problem isn't the configuration because I can open the socket via AT commands. Does any one have any idea of how can I fix it?
I'm using the 7.02.403 firmware version.
If there is any other relevant information that you need to think about the solution, just ask. But remember that I can connect via AT commands.
Code: Select all
I still have to check the century_data, but it doesn't matter now...import MDM
import MOD
import SER
def delay_s(seg):
MOD.sleep(seg*10)
def delay_m(min):
while min > 0:
delay_s(60)
min = min - 1
def send_TX(text):
a = SER.send(text)
if a != 1:
a = SER.send(text)
a = SER.sendbyte(13)
a = SER.sendbyte(10)
def send_AT(text):
a = MDM.send(text + '\r',0)
if a != 1:
a = MDM.send(text + '\r',0)
def receive_AT(timeout):
return MDM.receive(timeout*10)
def init():
send_AT('ATE0')
a = SER.set_speed('9600','8N1')
def skt_config():
send_AT('AT#PKTSZ=300')
send_AT('AT#DSTO=50')
send_AT('AT#SKTTO=90')
send_AT('AT#SKTCT=600')
send_AT('AT#USERID=EasyGPRS')
send_AT('AT#PASSW=EasyGPRS')
send_AT('AT+CGDCONT=1,"IP","tim.br",,,')
send_AT('AT#SKTSET=1,1720,"200.246.118.2",255,1025')
def connect_GPRS():
send_AT('AT#GPRS=1')
send_TX('AT#GPRS=1')
def check_GPRS():
send_AT('AT#GPRS?')
b = receive_AT(2)
if b.find('#GPRS: 1') != -1:
send_TX('GPRS: OK!')
return 1
else :
send_TX('GPRS: ERROR!!')
return 0
def open_SKT():
send_TX('AT#SKTOP')
send_AT('AT#SKTOP')
def close_SKT():
send_AT('+++')
def send_GPS_data():
send_AT('AT$GPSACP')
b = receive_AT(2)
c = 0
comma = 0
while c < len(b):
if b[c] == ':':
hora = b[c+2:c+8]
if b[c] == ',':
if comma == 0:
latitude = b[c+1:c+10]
if b[c+10] == 'S':
latitude = '-' + latitude
else :
latitude = '+' + latitude
elif comma == 1:
longitude = b[c+1:c+11]
if b[c+11] == 'W':
longitude = '-' + longitude
else :
longitude = '+' + longitude
elif comma == 8:
data = b[c+1:c+7]
comma = comma + 1
c = c+1
data = data[0:2] + '/' + data[2:4] + '/' + data[4:6]
hora = hora[0:2] + ':' + hora[2:4] + ':' + hora[4:6]
lat = latitude
lon = longitude
century_data = '$century,ID,'+hora+','+lat+','+lon+','+data
send_AT(century_data)
send_TX(century_data)
def main():
delay_s(2)
init()
skt_config()
send = 0
while 1:
if send == 1:
delay_m(1)
send = 0
if check_GPRS() == 0:
send_TX('connecting...')
connect_GPRS()
delay_s(5)
else :
open_SKT()
delay_s(2)
send_GPS_data()
close_SKT()
send = 1
Thanks!!
Copernicus