- Thu Aug 23, 2007 6:41 am
#34150
Thanx...
Leon.
I manage to do in way but got some problem. would u help me on this issue.Also i have put that issue in a other thread..
I have followed below the mentioned steps to communicate with web service . When i have connect the module in my PC ,got a COM3 port .Started proceeding with desired steps but had got a problem that the module is turned off( status green light not blinking) .
If i disconnected the antenna ,it proceeds up to the steps ,have proceeded,but whenever i am connecting the antenna with that module the status light (green light) stops blinking after 7-8 times it blinked and after that not able to write in the hyperterminal.
Steps Followed----
--> After putting a valid SIM card with GPRS enable in the Telit Module.
1. Hyper Terminal Setting:--
-> Open the Hyperterminal .Set a name and an icon for the connection.
->. Then in Connect to dialog box, choose the COM3 port which is come after connecting the EVK V3 module with the PC.
->Set in the Properties dialog box
Bits per second field = 9600
Data bits=8
Parity=None
Stop bit=1.
Flow control =Hardware .
->Then in Main Window of the Hyper terminal File->Properties menu, set the ASCII Setup as Echo typed locally.
2.EVK V3 Module Setting:--
Power On the Switch. Status light starts blinking.
3.AT COMMANDS TYPE in Hyperterminal:-
1.AT
Return: OK
2.AT+CPIN?
Return: REDDY
2.AT+CGDCONT=1,"IP","airtelgprs.com","0.0.0.0",0,0<cr>
Return: OK
3.AT#USERID="Easy GPRS"<cr>
Return: OK
4.AT#PASSWD="*****"<cr>
Return: OK
5.AT#PKTSZ=300
Return: OK
6.AT#DSTO=50
Return: OK
7.AT#SKTTO=90
Return: OK
8.AT#SKTCT=600
Return: OK
9.AT#SKTSAV
10..AT#GPRS=1<cr>