- Tue Jun 26, 2007 3:50 pm
#31875
You might be interested in the next release of this project. Figures show that the built-in CSV binary compressed storage format can reduce 59.4MiB of KML data to 7.9MiB. There's a bunch of other features too. Go straight to the userguides and downloads at http://gpslogger.blogspot.com now.
In other news, I'm now working for Google (completely unrelated to this project and not in an engineering role!) so geo-location is even closer to my heart!
---
I'm really pleased to announce release V0.94 of the GPS Logger MG for Spark Fun GPS Datalogger V1.0 (Trimble Lassen iQ) and V2.4 (US GlobalSat EM-406).
This release includes the following highlights:
- firmware now supports the Spark Fun GPS Datalogger V2.4 (EM-406) as well as the original V1.0 (Lassen iQ).
- emulator now provided for Linux 2.6 as well as FreeBSD 6 systems, and now works with either raw FAT images or standard file system I/O.
- compressed output, both generic LZARI based and specific CSV binary encoding, implemented to substantially reduce card writes and sizes thus improve power efficiency. code for two standalone decompression tools (perl & 'C') provided. performance against large sample sets fully evaluated and documented.
- provided a new 'passthrough' serial mode, for real-time direct GPS output to other devices, e.g. a PC. verified compatibility testing with numerous PC based applications (e.g. Microsoft AutoRoute 2007, Google Earth, NetStumbler, etc).
- various under-the-cover power, performance and feature improvements, e.g. data structures optimised to reduce RAM footprint, brown-out shutdown triggering, input data robustness (both GPS & config), lazy FAT cluster map updates, uart IRQ handling, timer delta-queue implementation, etc. code profiling also used.
- improved test coverage, with more built-in unit-test cases, greater splint and compiler verification (under both FreeBSD and Linux), and evaluation against large sample sets.
The complete details, with other features and changes not listed here, about the release, its installation and its use, can be found in the userguide.
The package and userguide are available for download from the project blog at http://gpslogger.blogspot.com.
This is V0.94 release. If any issues need to be rectified, then I plan to make an intermediate V0.95 release within a few weeks. Timely feedback would help!
The roadmap from there is to aim for a V0.96 release to focus on restructuring and improving the GPS data processing pipeline, with the capability to directly configure the GPS module for use. Following this, a V0.98 will focus on power and performance optimisation.
In other news, I'm now working for Google (completely unrelated to this project and not in an engineering role!) so geo-location is even closer to my heart!
---
I'm really pleased to announce release V0.94 of the GPS Logger MG for Spark Fun GPS Datalogger V1.0 (Trimble Lassen iQ) and V2.4 (US GlobalSat EM-406).
This release includes the following highlights:
- firmware now supports the Spark Fun GPS Datalogger V2.4 (EM-406) as well as the original V1.0 (Lassen iQ).
- emulator now provided for Linux 2.6 as well as FreeBSD 6 systems, and now works with either raw FAT images or standard file system I/O.
- compressed output, both generic LZARI based and specific CSV binary encoding, implemented to substantially reduce card writes and sizes thus improve power efficiency. code for two standalone decompression tools (perl & 'C') provided. performance against large sample sets fully evaluated and documented.
- provided a new 'passthrough' serial mode, for real-time direct GPS output to other devices, e.g. a PC. verified compatibility testing with numerous PC based applications (e.g. Microsoft AutoRoute 2007, Google Earth, NetStumbler, etc).
- various under-the-cover power, performance and feature improvements, e.g. data structures optimised to reduce RAM footprint, brown-out shutdown triggering, input data robustness (both GPS & config), lazy FAT cluster map updates, uart IRQ handling, timer delta-queue implementation, etc. code profiling also used.
- improved test coverage, with more built-in unit-test cases, greater splint and compiler verification (under both FreeBSD and Linux), and evaluation against large sample sets.
The complete details, with other features and changes not listed here, about the release, its installation and its use, can be found in the userguide.
The package and userguide are available for download from the project blog at http://gpslogger.blogspot.com.
This is V0.94 release. If any issues need to be rectified, then I plan to make an intermediate V0.95 release within a few weeks. Timely feedback would help!
The roadmap from there is to aim for a V0.96 release to focus on restructuring and improving the GPS data processing pipeline, with the capability to directly configure the GPS module for use. Following this, a V0.98 will focus on power and performance optimisation.