[phpBB Debug] PHP Warning: in file /mnt/forum-shared/ext/sitesplat/BBCore/event/listener.php on line 70: in_array() expects parameter 2 to be array, boolean given
GPS Datalogger v2.4 - SparkFun Electronics

SparkFun Forums 

Where electronics enthusiasts find answers.

Tips and questions relating to the GPS modules from SFE
By mikebres
#29743
Note: This is also posted in the Spark Fun Site Questions/Comments forum. I wasn't getting any answers there so now I trying this location. :)

I'm just starting with the Data Logger. It seems to work fine with the default settings.
So, now I'm working through the instructions and it says I can set the messages it will log by setting the Mode to 1 in the in the GLOGCON.TXT file on the SD card. So I set the following configuration where I only changed the mode from 0 to 1 everything else is default:
Mode = 1
Log What = RMC;GGA;GSA
Time Between Logs = 00:10:00
Holdoff = 5

now I get a solid blue LED on the logger board and nothing is logged.

Anybody know what I am doing wrong?

HELP!
Mike
By christophlorenz
#29954
Hi,

I have the same problem with the Logger. It seems it is not specific to a singel board.

Hope we get an answer from Sparkfun!

Regards Christoph
By Pete-O
#30335
Hi Guys...

I just happened to be browsing around here when I came upon your thread. The Blue LED is going to stay on while it waits for the EM-406 to get a lock. You'll know when that happens because the red LED on the EM-406 will start blinking. Does that help?

Pete