[phpBB Debug] PHP Warning: in file /mnt/forum-shared/ext/sitesplat/BBCore/event/listener.php on line 70: in_array() expects parameter 2 to be array, boolean given
GM862-GPS AT#CAMON Error - SparkFun Electronics

SparkFun Forums 

Where electronics enthusiasts find answers.

Tips and questions relating to the GPS modules from SFE
By foxxjnm
#24134
i just got the gm862-gps eval kit in along with the TC5747 cam + breakout. Everything works great on the module except for the camera commands. this is what i get for all camera commands:

at#camon
+CME ERROR: operation not supported

anyone else experiencing this? am i doing something wrong?

any response is appreciated!
Last edited by foxxjnm on Thu Dec 28, 2006 7:58 am, edited 1 time in total.
By foxxjnm
#24218
Anyone??
By muthas
#25899
yeah, same here... check out the GM862 product description, pg 67...

#CAMON and #CAMOFF aren't supported on the -GPS module. I think you're supposed to use the #CAMEN command to turn it on/off, but for me that doesn't work.

Did you buy the GM862 w/ a full eval board (rs232 or usb)? I just got the normal breakout board (just SMT to header pins) and wired up the level converter & camera interface myself... when I try to use the #CAMEN=1 command, I just get "+CME Error: Camera Initialization Error"

Let me know if the #CAMEN works for you...
By foxxjnm
#25900
I did get it working, and you are correct you must use CAMEN. I am using the V3 of the serial eval board.

Too bad the TC5747 has been discontinued, it worked well.
By siliconwee
#28273
HI, I connect a CMOS camera to GM862 as well, then using AT#CAMON AND AT#TPHOTO, all response ERROR. But ,

AT#CAMEN

#CAMEN: 0

OK

But, when i type AT#TPHOTO, the response as below
AT#TPHOTO

ERROR

So, who hv face this same problem?? foxxjnm and muthas , what do u think abt my problems? any suggestion??
thanks!

Nicole
By maokh
#28354
Have you guys tried to turn off the GPS first? Its on by default and you cannot have both turned on at once.
By siliconwee
#28372
hi, ya i hv disconnected the GPRS , but i stil cant turn on the CMOS camera. Actually i hv refer to the Telit website, cos my GM862 is bought from there. What i discover is all telit module , the supported camera is Agilent ADCM2650 or the Transchip TC5747. i think if i want to connect the CMOS camera to the module, hv to do a controller external circuit.

Nicole