Problem PPS signal Venus GPS

Tips and questions relating to the GPS modules from SFE

Moderator: phalanx

Post Reply
powergravity
Posts: 3
Joined: Mon Nov 28, 2016 8:07 am

Problem PPS signal Venus GPS

Post by powergravity » Thu Jun 01, 2017 1:17 am

Hello,

I am realizing that the PPS pin of my Venus GPS doesn't send any signal. I am not able to make it work....

After having read the data sheet of the GPS, I saw :
Image

Hence I try to send the following message to the GPS:

Code: Select all

   // PPS message:
   byte PPSmessage[] = {0xA0, 0xA1, 0x00, 0x03, 0x3E, 0x01, 0x01, 0x3E, 0x0D, 0x0A};  
   gps_port.write( PPSmessage, sizeof(PPSmessage) );                                  
   gps_port.flush();                                                                           
but nothing changes.

Is there someone who has ever had a similar problem?

Thank you in advance,
Pm

gm
Posts: 202
Joined: Fri May 04, 2007 3:08 pm

Re: Problem PPS signal Venus GPS

Post by gm » Fri Jun 02, 2017 9:01 am

Perhaps the checksum is wrong. It appears that you just copied the value from the example but have changed the values for fields 1 and 2.

powergravity
Posts: 3
Joined: Mon Nov 28, 2016 8:07 am

Re: Problem PPS signal Venus GPS

Post by powergravity » Fri Jun 02, 2017 10:24 am

Thants for your answer. I don't think that the problem comes from the CS because [0x01 0x01] leads to the same CS than with [0x00 0x00], right?

Have a good day,
Pm

Valen
Support Volunteer
Posts: 1628
Joined: Wed Dec 22, 2010 2:05 am

Re: Problem PPS signal Venus GPS

Post by Valen » Sat Jun 03, 2017 2:52 am

In general, a checksum is the summation of a number of bytes. And then of the final sum only the least significant byte is used. Any higher significant bytes are discarded. Sometime the final byte is bit-inverted or subtracted from a constant or XOR-ed with a constant before inserting it in the datastream.

In your example [0x01, 0x01] a checksum would be 0x02. For [0x00, 0x00] its 0x00. The example above calculates the checksum to be 0x3E for the sequence [0x3E, 0x00,0x00]. It implies the MessageID is supposed to be included for the checksum. The piece of text that you show does not explain the finer details of how the checksum is to be calculated. And I haven't read it's manual. So make sure to check.

Post Reply