- Wed Jun 26, 2013 3:22 am
#160957
I've never played with GPS before, bought the logger quite a while ago, just now starting to tinker with it.
I'm using AF's 128x64 OLED display, a Teensy 3.0, The venus logger SMA, SMA antenna (non-housed), and a 3V3 FTDI cable.
Sitting at my desk, my phone can fix on 6 birds.
I loaded the TinyGPS lib, got the display to work, and got things to "seemingly" behave.
But the GPS won't fix? It just keeps saying 0 satellites. I plug my FTDI into the loop to see the NMEA strings (which i had to look up to debug), and they all say V/Void in the validity term.
Am I missing anything, or does it just not want to fix? I set it in a south facing window for 30 minutes, and the LED was still solid green, and display showed 0 birds.
I'm using AF's 128x64 OLED display, a Teensy 3.0, The venus logger SMA, SMA antenna (non-housed), and a 3V3 FTDI cable.
Sitting at my desk, my phone can fix on 6 birds.
I loaded the TinyGPS lib, got the display to work, and got things to "seemingly" behave.
But the GPS won't fix? It just keeps saying 0 satellites. I plug my FTDI into the loop to see the NMEA strings (which i had to look up to debug), and they all say V/Void in the validity term.
Am I missing anything, or does it just not want to fix? I set it in a south facing window for 30 minutes, and the LED was still solid green, and display showed 0 birds.
Code: Select all
#include <Wire.h>
#include <Adafruit_GFX.h>
#include <Adafruit_SSD1306.h>
#include <TinyGPS.h>
#define OLED_DC 21
#define OLED_CS 10
#define OLED_CLK 13
#define OLED_MOSI 11
#define OLED_RESET 9
Adafruit_SSD1306 display(OLED_MOSI, OLED_CLK, OLED_DC, OLED_RESET, OLED_CS);
#if (SSD1306_LCDHEIGHT != 64)
#error("Height incorrect, please fix Adafruit_SSD1306.h!");
#endif
TinyGPS gps;
elapsedMillis checkData;
void setup() {
// by default, we'll generate the high voltage from the 3.3v line internally! (neat!)
display.begin(SSD1306_SWITCHCAPVCC);
Serial1.begin(9600);
// init done
display.display(); // show splashscreen
delay(2000);
display.clearDisplay(); // clears the screen and buffer
// text display tests
display.setTextSize(1);
display.setTextColor(WHITE);
display.setCursor(0,0);
display.print("Simple TinyGPS library v. ");
display.println(TinyGPS::library_version());
display.println("by Mikal Hart");
display.display();
delay(1000);
display.clearDisplay(); // clears the screen and buffer
display.display();
display.setCursor(0,0);
}
int printCount = 0;
void loop() {
bool newData = false;
unsigned long chars;
unsigned short sentences, failed;
// For one second we parse GPS data and report some key values
for (unsigned long start = millis(); millis() - start < 1000;)
{
//display.print("a");
while (Serial1.available())
{
//display.print("b");
char c = Serial1.read();
display.print(c); // uncomment this line if you want to see the GPS data flowing
if (gps.encode(c)){ // Did a new valid sentence come in?
//display.print("c");
newData = true;
display.display();
}
}
}
if (checkData > 1000){
checkData = checkData - 1000;
display.clearDisplay(); // clears the screen and buffer
display.setCursor(0,0);
display.display();
}
float flat, flon;
unsigned long age;
gps.f_get_position(&flat, &flon, &age);
display.print("LAT=");
display.println(flat == TinyGPS::GPS_INVALID_F_ANGLE ? 0.0 : flat, 6);
display.print(" LON=");
display.println(flon == TinyGPS::GPS_INVALID_F_ANGLE ? 0.0 : flon, 6);
display.print(" SAT=");
display.println(gps.satellites() == TinyGPS::GPS_INVALID_SATELLITES ? 0 : gps.satellites());
display.display();
}