- Thu Apr 25, 2013 2:36 am
#158855
Hi guys,
I am using a GPS em-406a connected on an Arduino UNO and it does not receive any coordinates.
Please see below my code:
Regarding the GPS, It does NOT enter the "while (gpsss.available())" loop. I have also tried "Serial.print(gpsss.read());" and it prints "-1".
Although im a rookie on these stuff, I am sure that my connections are correct ----> pin 1&5 = GND, pin 2 = VIN, pin 3 = Rx, pin 4 = Tx
and I have connected them to respective pin on the arduino -----> GND = GND, VIN = 5V, Rx = pin 4, Tx = pin 5
Any ideas of how to resolve this problem would be most appreciated.
Thank you in advance,
gabys
I am using a GPS em-406a connected on an Arduino UNO and it does not receive any coordinates.
Please see below my code:
#include <XBee.h>I am also using an xbee module which is working fine. I have also commented out some of the code and left only the critical part of it.
#include <TinyGPS.h>
#include <SoftwareSerial.h>
// Define SoftwareSerial TX/RX pins
#define xbeeRX 2
#define xbeeTX 3
#define gpsRX 4
#define gpsTX 5
//create xbee connection
SoftwareSerial xbeess = SoftwareSerial(xbeeRX, xbeeTX);
//create gps connection
SoftwareSerial gpsss = SoftwareSerial (gpsRX, gpsTX);
//Create an XBee object
XBee xbee = XBee();
TinyGPS gps;
//Define the Destination address of the packets
XBeeAddress64 destaddress = XBeeAddress64(0x0013A200, 0x406F1997);
char Hello[] = "Hello World\n\r";
void setup()
{
Serial.begin(9600); //connect serial
xbeess.begin(9600); //connect xbee
gpsss.begin(4800); //connect gps
//We hook the XBee into the Software Serial
xbee.setSerial(xbeess);
Serial.println("Goodnight moon!");
}
void loop() // run over and over
{
/*long flat, flon;
gps.get_position(&flat, &flon);
char* lat;
sprintf(lat, "%f", flat);
char* lon;
sprintf(lon, "%f", flon);*/
Serial.println("in the loop");
while (gpsss.available()){
Serial.println("fail");
if (gps.encode(gpsss.read())){
Serial.println("hello");
//Serial.println(*lat + " " + *lon);
}
}
ZBTxRequest zbtx = ZBTxRequest(destaddress, (uint8_t *)Hello, strlen(Hello));
xbee.send(zbtx);
delay(1000);
}
Regarding the GPS, It does NOT enter the "while (gpsss.available())" loop. I have also tried "Serial.print(gpsss.read());" and it prints "-1".
Although im a rookie on these stuff, I am sure that my connections are correct ----> pin 1&5 = GND, pin 2 = VIN, pin 3 = Rx, pin 4 = Tx
and I have connected them to respective pin on the arduino -----> GND = GND, VIN = 5V, Rx = pin 4, Tx = pin 5
Any ideas of how to resolve this problem would be most appreciated.
Thank you in advance,
gabys