SparkFun Forums 

Where electronics enthusiasts find answers.

Tips and questions relating to the GPS modules from SFE
By blen
#158117
I recently read about vehicle to vehicle (V2V) GPS in popular mechanics. Is there any such device(s) * available* as far as smaller GPS units that talk to each other, like between 3 devices to triangulate positions, etc? I am clueless and at your mercy, thanks. :think:
By SFE-Toni
#158759
I'm not aware of any GPS units by themselves that communicate back and forth, but you could hook up a few gps units to an Xbee network and transmit data back and forth that way.
By blen
#159668
Thanks guys. The units need to be able to communicate w/each other. One is a home base stationary unit if you will, the other two are mobile. All 3 need to be able to communicate w/each other in real time and I am looking for devices that are accurate from 1 ft-40 ft if something like this exists....
By jremington
#159671
That article is five years old! High-accuracy (better than 1 m resolution) commercial GPS units that use a nearby base station are readily available. Expect to pay >$1000 for such a unit. But why would you want the units to talk to each other?
By nickersonm
#159721
That article doesn't involve exchange of GPS information, but rather the systems with the GPS units sending data to a central source that guess traffic, etc. from the various speeds and positions.