- Thu Nov 08, 2012 8:14 pm
#151508
Hi, hoping someone could help, I have connected the GPS LS20031 & Open logger to make a tracker, my under standing was after powering them up, I just go for a walk then when finest turn them off. I then should be able to just remove the sim card put it into my PC & open the log file. Now this is were I get stuck, the log file is a text Doc when I open it in note pad I don't know what code it is, my under standing is the GPS should log the info in a NMEA format (witch is not happening) you can then import it in to Google earth & Google makes it into a KLM file were you can see were you have been going.
Not sure were I have gone wrong. Do I need to change a setting or convert the text file to NMEA? the sim card is FAT32 and the only contection that I left of the GPS to the logger was the GPS RX input & the TX0 output on the logger.
Regards Goobs
Not sure were I have gone wrong. Do I need to change a setting or convert the text file to NMEA? the sim card is FAT32 and the only contection that I left of the GPS to the logger was the GPS RX input & the TX0 output on the logger.
Regards Goobs