- Wed Sep 26, 2012 4:11 am
#149859
Hello!! First post!! I've just received the Trimble Lassen IQ module i ordered form Sparkfun. I connected the module to Arduino board and i'm able to receive and process GGA strings. I need to use the module for a high altitude balloon flight, so i need to be sure that there isn't limit for altitude measurement.
I read on the datasheet that the limit for altitude is 18000 m and the speed limit is 515 m/s. The question is: have i to configure the module to allow altitude measurement without limits? If yes, how? I can't find anywhere this procedure! :think:
Thanks for your attention!!
I read on the datasheet that the limit for altitude is 18000 m and the speed limit is 515 m/s. The question is: have i to configure the module to allow altitude measurement without limits? If yes, how? I can't find anywhere this procedure! :think:
Thanks for your attention!!