- Thu Jun 07, 2012 10:53 am
#145641
I am using an Adafruit Ultimate GPS Breakout (66 channel w/10 Hz updates - MTK3339 chipset) unit and mounting it to a ski helmet. The arduino is is going to be either in a backpack or fannypack. In either case there will be a cable run of several feet between the GPS module and the arduino.
I am putting the GPS module on the helmet to assure it pointing up. Maybe I don't need to do that and it will work fine in the either pack. But, I think I will get a more reliable signal from a helmet mount.
Any advice on this? It's a serial connection via the tx and rx ports. Do I need to worry about noise in the line if it is up to 3 ft. long? If so how can I design for it?
Thanks!
I am putting the GPS module on the helmet to assure it pointing up. Maybe I don't need to do that and it will work fine in the either pack. But, I think I will get a more reliable signal from a helmet mount.
Any advice on this? It's a serial connection via the tx and rx ports. Do I need to worry about noise in the line if it is up to 3 ft. long? If so how can I design for it?
Thanks!