- Thu Jan 05, 2012 11:14 am
#137838
Hi there,
I purchased a EM-408 GPS Module (http://www.sparkfun.com/products/8234) and can`t make it working.
Im trying to get it running with an Arduino UNO (ATMEGA 328) and the tinyGPS Library.
The VCC is connected to 3.3V, GND to Ground, RX to Pin 0 and TX to Pin 1.
Enable/Disable is connected to 3.3V through a 4.7K Resistor and should therefore be HIGH
(my knowledge in electrics is very basic).
The Arduino receives no data from the module (RX LED is LOW).
Did anybody experience similar problems with the EM-408?
I found this: viewtopic.php?t=6623
and this: http://geoffg.net/EM408.html
but couldn`t solve my problem.
heres the Code (its a slightly modified tinyGPS Example and compiles only with Arduino 0022)
zonk
I purchased a EM-408 GPS Module (http://www.sparkfun.com/products/8234) and can`t make it working.
Im trying to get it running with an Arduino UNO (ATMEGA 328) and the tinyGPS Library.
The VCC is connected to 3.3V, GND to Ground, RX to Pin 0 and TX to Pin 1.
Enable/Disable is connected to 3.3V through a 4.7K Resistor and should therefore be HIGH
(my knowledge in electrics is very basic).
The Arduino receives no data from the module (RX LED is LOW).
Did anybody experience similar problems with the EM-408?
I found this: viewtopic.php?t=6623
and this: http://geoffg.net/EM408.html
but couldn`t solve my problem.
heres the Code (its a slightly modified tinyGPS Example and compiles only with Arduino 0022)
Code: Select all
thanks for any answers#include <NewSoftSerial.h>
#include <TinyGPS.h>
/* This sample code demonstrates the normal use of a TinyGPS object.
It requires the use of NewSoftSerial, and assumes that you have a
4800-baud serial GPS device hooked up on pins 0(rx) and 1(tx).
*/
TinyGPS gps;
NewSoftSerial nss(0, 1);
void gpsdump(TinyGPS &gps);
bool feedgps();
void printFloat(double f, int digits = 2);
void setup()
{
Serial.begin(9600);
nss.begin(4800);
pinMode(13,OUTPUT);
Serial.print("Testing TinyGPS library v. "); Serial.println(TinyGPS::library_version());
Serial.println("by Mikal Hart");
Serial.println();
Serial.print("Sizeof(gpsobject) = "); Serial.println(sizeof(TinyGPS));
Serial.println();
}
void loop()
{
bool newdata = false;
unsigned long start = millis();
digitalWrite(13,HIGH);
Serial.println("no Data");
// Every 5 seconds we print an update
while (millis() - start < 5000)
{
if (feedgps())
newdata = true;
}
if (newdata)
{
Serial.println("Acquired Data");
Serial.println("-------------");
gpsdump(gps);
Serial.println("-------------");
Serial.println();
}
}
void printFloat(double number, int digits)
{
// Handle negative numbers
if (number < 0.0)
{
Serial.print('-');
number = -number;
}
// Round correctly so that print(1.999, 2) prints as "2.00"
double rounding = 0.5;
for (uint8_t i=0; i<digits; ++i)
rounding /= 10.0;
number += rounding;
// Extract the integer part of the number and print it
unsigned long int_part = (unsigned long)number;
double remainder = number - (double)int_part;
Serial.print(int_part);
// Print the decimal point, but only if there are digits beyond
if (digits > 0)
Serial.print(".");
// Extract digits from the remainder one at a time
while (digits-- > 0)
{
remainder *= 10.0;
int toPrint = int(remainder);
Serial.print(toPrint);
remainder -= toPrint;
}
}
void gpsdump(TinyGPS &gps)
{
long lat, lon;
float flat, flon;
unsigned long age, date, time, chars;
int year;
byte month, day, hour, minute, second, hundredths;
unsigned short sentences, failed;
gps.get_position(&lat, &lon, &age);
Serial.print("Lat/Long(10^-5 deg): "); Serial.print(lat); Serial.print(", "); Serial.print(lon);
Serial.print(" Fix age: "); Serial.print(age); Serial.println("ms.");
feedgps(); // If we don't feed the gps during this long routine, we may drop characters and get checksum errors
gps.f_get_position(&flat, &flon, &age);
Serial.print("Lat/Long(float): "); printFloat(flat, 5); Serial.print(", "); printFloat(flon, 5);
Serial.print(" Fix age: "); Serial.print(age); Serial.println("ms.");
feedgps();
gps.get_datetime(&date, &time, &age);
Serial.print("Date(ddmmyy): "); Serial.print(date); Serial.print(" Time(hhmmsscc): "); Serial.print(time);
Serial.print(" Fix age: "); Serial.print(age); Serial.println("ms.");
feedgps();
gps.crack_datetime(&year, &month, &day, &hour, &minute, &second, &hundredths, &age);
Serial.print("Date: "); Serial.print(static_cast<int>(month)); Serial.print("/"); Serial.print(static_cast<int>(day)); Serial.print("/"); Serial.print(year);
Serial.print(" Time: "); Serial.print(static_cast<int>(hour)); Serial.print(":"); Serial.print(static_cast<int>(minute)); Serial.print(":"); Serial.print(static_cast<int>(second)); Serial.print("."); Serial.print(static_cast<int>(hundredths));
Serial.print(" Fix age: "); Serial.print(age); Serial.println("ms.");
feedgps();
Serial.print("Alt(cm): "); Serial.print(gps.altitude()); Serial.print(" Course(10^-2 deg): "); Serial.print(gps.course()); Serial.print(" Speed(10^-2 knots): "); Serial.println(gps.speed());
Serial.print("Alt(float): "); printFloat(gps.f_altitude()); Serial.print(" Course(float): "); printFloat(gps.f_course()); Serial.println();
Serial.print("Speed(knots): "); printFloat(gps.f_speed_knots()); Serial.print(" (mph): "); printFloat(gps.f_speed_mph());
Serial.print(" (mps): "); printFloat(gps.f_speed_mps()); Serial.print(" (kmph): "); printFloat(gps.f_speed_kmph()); Serial.println();
feedgps();
gps.stats(&chars, &sentences, &failed);
Serial.print("Stats: characters: "); Serial.print(chars); Serial.print(" sentences: "); Serial.print(sentences); Serial.print(" failed checksum: "); Serial.println(failed);
}
bool feedgps()
{
while (nss.available())
{
if (gps.encode(nss.read()))
return true;
}
return false;
}
zonk