SparkFun Forums 

Where electronics enthusiasts find answers.

Tips and questions relating to the GPS modules from SFE
By tld
#136044
I'm not an authority on anything here, as I'm starting out myself, but since you haven't gotten an answer yet...

Don't look at it as "interfacing with a gps module", but rather "getting a serial interface up". ;)

The gp 2106 needs 1.8V for power, and has 3.3V tolerant RX, so you could probably make things easier by powering your arduino at 3.3V, unless that conflicts with anything. I know the atmel chip can, and I don't see anything stopping it (unless you're powering from USB, and don't want to solder).

You could do something like:

Use a 3.3V regulator connected to the 5V pin of your Arduino.
Use a 1.8V regulator connected to Vin on the GPS.
Hook up serial lines directly between the GPS and Arduino.
Hook up a GPIO-pin to the on/off pin of the GPS, to start, shutdown or hibernate it (at least start).

NOTE: You want to check both the GPS and Voltage regulators for their capacitor needs. For voltage-regulators, bad things can happen if you skip them.

There are lots of serial tutorials for the Arduino, and lots of GPS-tutorials for dealing with the NMEA-sentances.

Done.

A bit simplified perhaps, but should give a starting point. Probably best to read the full datasheet, and ask if you have any questions.

tld