- Wed Aug 10, 2011 9:29 am
#131625
I am presently trying to imitate a Find Home Detector seen on Hackaday.com, with a couple improvements, but I'm having trouble getting a response from the GPS Minimod I'm using.
I have an LED ring (Mayhew labs) indicating the compass module readout and an LCD screen giving a text-based readout of the same bearing (for the moment, it'll show distance later on). I looked around for some code related to the Minimod that I could reverse engineer to get what I need, but it doesn't seem all that common.
Currently, the Minimod is hooked up to VCC to D24, Gnd on Gnd, and TX to D22 on my Arduino Mega 2560. What I need to find out are the coding requirements for using it, and ideally some code examples of its usage.
I have an LED ring (Mayhew labs) indicating the compass module readout and an LCD screen giving a text-based readout of the same bearing (for the moment, it'll show distance later on). I looked around for some code related to the Minimod that I could reverse engineer to get what I need, but it doesn't seem all that common.
Currently, the Minimod is hooked up to VCC to D24, Gnd on Gnd, and TX to D22 on my Arduino Mega 2560. What I need to find out are the coding requirements for using it, and ideally some code examples of its usage.
Code: Select all
This is the current code I'm working with, but all it ever returns is No data and the GPS lock LED never initiates.#include <NewSoftSerial.h>
#include <LiquidCrystal.h>
NewSoftSerial gps(22, 24);
LiquidCrystal lcd(7, 8, 9, 10, 11, 12);
void setup()
{
gps.begin(4800);
lcd.begin(16, 2);
Serial.begin(115200);
pinMode(5, OUTPUT);
analogWrite(5, 90);
pinMode(13, OUTPUT);
}
void loop()
{
lcd.clear();
if (gps.available()) {
lcd.print(gps.read(), BYTE);
}
else {
lcd.print("No data");
}
blink();
delay(1000);
}
void blink() {
digitalWrite(13, HIGH);
delay(100);
digitalWrite(13, LOW);
}