- Mon Apr 04, 2011 11:43 am
#124520
I have the Venus 634 with SMA board ( 4-27-09 ) currently connected
to a logomatic v2 via
GND > GND
3.3V > 3.3V
TX > RX
RX > TX
this all works fine and logs data.
My question is as the power from the logomatic is switched off the
venus board cold starts each time. I believe that if i de solder a
jumper ( not sure if this is the one next to the vbat pin ) and
connect the battery to this pin that it will warm start each time
instead?
Also if the above is correct, is there a permanent 3.3v available from
the logomatic board pins? or should i just feed of the power
connector?
Many Thanks
to a logomatic v2 via
GND > GND
3.3V > 3.3V
TX > RX
RX > TX
this all works fine and logs data.
My question is as the power from the logomatic is switched off the
venus board cold starts each time. I believe that if i de solder a
jumper ( not sure if this is the one next to the vbat pin ) and
connect the battery to this pin that it will warm start each time
instead?
Also if the above is correct, is there a permanent 3.3v available from
the logomatic board pins? or should i just feed of the power
connector?
Many Thanks