- Sun Feb 13, 2011 3:49 pm
#120186
Hey all, first time poster here.
I recently purchased the Copernicus DIP Module for use in a high altitude balloon project, having heard that it is known to function at over 100,000 ft. In the enourmous datasheet for this module, Trimble outlines the structure and function of their proprietary communication protocol, TSIP (Page 97). Being a relative newbie to this sort of thing, I was surprised at how easy it was to receive any data at all from it-- all I had to do was connect a handful pins to the Arduino Mega 2560 I'm using: a few to 3.3v Vcc, one to ground, and two for TX-A and RX-A*.
However, the data that I'm getting from the Copernicus doesn't seem to follow the format for TSIP packets which is described in the datasheet. At least, if it does, I can't see it. Here's the Arduino sketch I threw together to format the data nicely:
*(R/TX-A communicates with TSIP, while R/TX-B uses the standard NMEA protocol)
Thanks,
Yodel
I recently purchased the Copernicus DIP Module for use in a high altitude balloon project, having heard that it is known to function at over 100,000 ft. In the enourmous datasheet for this module, Trimble outlines the structure and function of their proprietary communication protocol, TSIP (Page 97). Being a relative newbie to this sort of thing, I was surprised at how easy it was to receive any data at all from it-- all I had to do was connect a handful pins to the Arduino Mega 2560 I'm using: a few to 3.3v Vcc, one to ground, and two for TX-A and RX-A*.
However, the data that I'm getting from the Copernicus doesn't seem to follow the format for TSIP packets which is described in the datasheet. At least, if it does, I can't see it. Here's the Arduino sketch I threw together to format the data nicely:
*(R/TX-A communicates with TSIP, while R/TX-B uses the standard NMEA protocol)
Code: Select all
Here's a sample of what I'm getting:
int newInput = 0; //The most recent thing read by serial3.
double clock; //Time read from Arduino's internal clock.
int prevClock; //Stores the last time valid data was recieved.
void setup()
{
Serial3.begin(4800);
Serial.begin(9600);
clock = millis();
}
void loop()
{
newInput = Serial3.read(); //Reads data from Copernicus pin TX-A.
if (newInput != -1)
{
prevClock = clock;
Serial.print(newInput, HEX); //Prints the decimal data as hex digits.
Serial.print(" ");
}
clock = millis(); //Records the time.
if (newInput == 255 || ((clock - prevClock) < 2 && newInput != -1) ) //Makes a new line if most recent data recieved was the
Serial.println("\n"); // hex number FF, or if there was a significant gap in the data transmission.
}
Code: Select all
Every line in the data above was transmitted at intervals of one second, and seemed to end relatively reliably with the hex digit FF (the times when it didn't are shown as longer data strings). Trimble's manual states that every packet of information begins with the "<DLE>" byte (0x10), and ends with an odd number of <DLE> bytes followed by an "<ETL>" byte (0x03). I don't see this anywhere in the data above... can anyone tell me what's going wrong here?63 2 0 0 2 40 0 0 E0 16 82 E1 48 10 0 1A FF
63 2 0 0 2 40 2 0 E0 56 82 E1 40 0 0 18 FF
3 2 40 0 2 0 2 2 E0 76 82 E2 3 0 2 7 FF
3 62 40 0 2 40 2 0 E0 56 82 B0 D0 0 2 7 FF
3 62 40 0 2 40 2 0 E0 36 82 D1 62 0 0 1A FF
3 62 40 0 2 40 2 0 E0 5E A2 C1 60 40 0 7 FF
3 40 40 0 2 2 2 0 E0 3A C0 E2 44 40 0 1A FF
3 42 40 0 2 40 42 0 E0 56 82 E1 44 0 40 1A FF
3 2 40 0 42 40 2 0 E0 16 82 E1 40 10 2 1A FF
63 62 0 0 2 40 2 0 E0 5E 83 E1 48 10 0 1A FF
3 2 40 0 2 40 2 0 E0 16 82 D1 60 0 0 7 FF
3 2 40 0 2 40 2 0 E0 76 83 D1 60 0 0 7 FF
3 0 40 0 2 0 2 2 E0 E 83 C1 60 0 0 1A FF
23 62 40 0 2 40 2 0 E2 66 82 E1 48 0 0 18 FF
3 2 0 0 2 40 2 0 E2 8 C0 E0 44 0 0 7 FF
3 2 2 0 0 40 2 40 E0 4E 83 D1 60 0 0 17 FF
3 2 0 0 2 40 2 0 E0 8 C0 E3 44 0 0 7 FF
1 2 0 0 2 40 0 0 E0 4E 82 C1 60 2 0 7 FF
1 2 0 0 2 40 2 0 E2 2E 82 C1 60 2 0 7 FF
23 2 40 2 2 0 2 0 E0 46 82 C1 60 0 0 1A FF
63 2 40 0 2 40 2 0 E0 26 82 E1 44 2 0 7 FF
23 62 40 0 2 40 2 0 E0 4A C0 E3 44 40 0 1A FF
1 2 40 0 2 40 2 0 E2 E 22 11 6A 0 2 93 3 62 40 0 2 40 2 0 E0 4A A2 E1 40 10 0 1A FF
3 2 2 0 2 40 2 40 E0 1E 83 B0 D0 2 40 7 FF
3 62 40 0 2 40 42 0 E0 7E A2 C1 60 2 40 7 FF
3 62 40 0 2 40 2 0 E0 16 83 E0 44 0 0 1A FF
3 62 40 2 2 40 2 0 E0 46 82 E1 44 0 0 1A FF
3 62 40 0 2 40 42 0 E0 6 82 C1 60 0 0 1A FF
3 2 2 0 0 40 2 40 E0 46 22 51 D2 0 0 7 FF
1 2 2 0 2 40 2 40 E0 E 83 C1 44 40 0 17 FF
3 2 40 0 2 40 2 0 E0 4A C0 62 48 0 40 1A FF
3 2 0 0 2 40 2 40 E0 3A C0 62 48 0 40 1A FF
1 2 0 0 2 40 2 40 E0 46 82 D1 60 0 0 7 FF
3 42 40 0 2 40 42 0 E0 26 2 51 D0 0 0 7 FF
1 2 0 0 2 C0 2 0 E0 5E 82 D1 E0 0 2 17 FF
1 2 40 0 2 40 2 0 E0 16 83 D1 60 0 40 7 FF
1 2 40 0 2 40 2 0 E0 56 82 E3 44 40 0 1A FF
41 2 40 40 2 0 2 0 E0 18 C0 62 48 0 0 1A FF
41 2 40 40 2 0 2 0 E0 78 C0 60 44 0 0 1A FF
63 2 0 0 2 40 0 0 E0 16 82 D1 E0 40 0 7 FF
41 2 0 0 2 40 0 0 E0 76 82 E1 40 0 0 1A FF
1 2 40 40 2 0 2 0 E0 18 C0 E3 41 0 0 7 FF
3 2 40 0 2 40 42 0 E0 58 C0 E3 44 0 0 1A FF
3 2 0 0 2 40 2 40 E0 46 82 B0 D0 2 40 7 FF
3 2 40 0 2 0 2 0 E0 48 C0 60 44 0 0 1A FF
3 0 40 0 42 40 2 0 60 6D F0 E3 44 2 40 7 FF
63 2 0 0 2 40 0 0 E0 26 22 1 6A 0 0 93 23 62 40 0 2 2 2 2 E0 26 2 51 D0 0 0 7 FF
63 2 0 0 2 40 2 0 E0 6 22 51 2A 0 2 93 3 62 40 2 2 40 2 0 E0 46 82 E0 44 0 0 7 FF
63 2 0 0 2 40 2 0 E0 4E 82 E0 44 0 0 1A FF
3 42 40 0 2 40 42 0 E0 8 C0 60 44 0 40 7 FF
23 2 40 0 2 2 2 0 E0 68 C4 62 44 40 0 1A FF
3 40 40 0 2 2 2 0 E0 76 82 60 44 0 0 7 FF
23 2 40 0 2 2 2 0 E0 76 82 C1 60 0 0 1A FF
3 2 40 0 42 40 2 0 E0 16 82 E1 48 0 0 1A FF
3 62 40 0 2 40 2 0 E0 5E 82 C1 62 0 0 1A FF
3 62 2 0 0 40 2 0 E0 1A 22 51 D0 40 0 17 FF
3 2 0 0 2 40 2 40 E0 56 82 D1 60 0 2 7 FF
3 2 40 0 2 40 42 0 E0 26 82 D1 60 0 2 7 FF
3 2 40 0 2 40 42 0 E0 4E 40 B2 D0 40 0 7 FF
3 2 2 0 0 40 2 40 E0 2A C0 E1 44 40 0 1A FF
1 2 40 0 2 40 2 0 E0 46 83 E1 44 0 40 1A FF
3 2 40 0 42 40 2 0 E0 16 A2 C1 60 0 0 7 FF
1 2 40 0 42 40 2 0 E0 56 83 E1 48 0 0 1A FF
23 62 0 0 2 40 2 0 2 7 44 1 3 2 60 F4 3 2 40 0 2 40 2 0 E2 7E 83 D1 60 0 0 7 FF
3 2 0 0 2 40 2 0 E2 5E 40 B0 D2 0 2 17 FF
3 62 40 0 2 40 42 0 E0 78 C0 E1 44 0 2 7 FF
Thanks,
Yodel