mike whorley wrote:the rule for altitude records (flawed as it maybe) states that flights over 30,000 ft altitude needs to be determined by gps.
According to Wikipedia: GPS,
"All GPS receivers capable of functioning above 18 kilometers (11 mi) altitude and 515 metres per second (1,001 kn) [3] are classified as munitions (weapons) ... These limits attempt to prevent use of a receiver in a ballistic missile. ... This rule applies even to otherwise purely civilian units ... Disabling operation above these limits exempts the receiver from classification as a munition. Vendor interpretations differ. ... This has caused problems with some amateur radio balloon launches which regularly reach 30 kilometers (19 mi)."
Is there any way to tell if your GPS is deliberately choosing not to work in an attempt to avoid the munitions classification, and is perhaps being excessively conservative?