SparkFun Forums 

Where electronics enthusiasts find answers.

Tips and questions relating to the GPS modules from SFE
#96747
Hi All,

Rant on
I received LS23060 GPS Receiver instead of the 32 Channel LS20031 GPS 5Hz Receiver I ordered.
They say it is the LS20031 GPS 5Hz Receiver I ordered event though the pictures I sent them show something different. Twice in one month I have not recieved what I ordered from this company.
Off Rant

Problem,
I can't get the reciever to send clear text showing the NMEA data being sent to RealTerm.
Tried different baud rate settings both on the PC and on the GPS. Nothing seems to be working.
I have attached an image of what I'm seeing in the RealTerm window.
realterm_error.jpg
Anyone have any ideas what I can do to fix this issue?

Thanks
Don Anderson
You do not have the required permissions to view the files attached to this post.
By Polux rsv
#96776
Yes, bad connection: ground connection, level converter problem. See bottom of your display: UART receiver framing error.

Or the classic :
-Hey, I connected my GPS unit directly to the RS232 port, and it doesn't work !!! :oops:
-How do you connect it ? :roll:
- As usual, GND on GND, Tx on unit to RS232 Rx, and Rx to Tx :x
- And what about a level converter, or usb to TTL serial ? :lol:
- What are you talking about ? :?
- You can't connect directly a device with TTL level outputs to a RS232 interface. :wink:
- And how can I make it working ? :(
- Use a simple MAX232. Or connect your GPS to a USB to TTL serial cable :D
- Ok, I will try this. Thanks :P
- Ok, who's next ? :mrgreen:

Ok, Ok, dont't push me, I see the exit, I could go by myself :mrgreen: :arrow:

Angelo
#96945
Hey All,
Thanks for the quick replys.
It turns out there is a issue with the FTDI cable I was using that was part of the problem.

Anyone have an idea on a way to configure the GPS so I do not get a CRLF at the end of each line?
RealTerm_error2.jpg
Thanks for any help you can provide.
Don Anderson
You do not have the required permissions to view the files attached to this post.
#97016
Good point.
The CrLF would be a good marker to show the end of one set of values.
Was not thinking of that. Just thinking of the microcontroller not having to deal with processing the extra charecters. The microcontroller will be comunicating with another microcontroller and at some
point I plann to have main controller recording data from 12 or more sensors.
Thanks for helping me open my sights :-)
By e-samolocik
#102621
Hi All,

Just couple of days ago, mistakenly I have inverted Ground and Power cables and connected my Locosys LS20031 gps.
In resoult something burned. It doesn't power up anymore.
Does anyone know if this can be fixed?

Is there any resistor that i can exchange and bring my GPS back to life?

I would be thankful for any help.