SparkFun Forums 

Where electronics enthusiasts find answers.

Tips and questions relating to the GPS modules from SFE
By microera
#57796
Hi
I read many times this:
http://www.gpsgate.com/index.php?id=92
and I think setting all ok but can't connect to my user "telit8305" on gpsgate!
I have at moment this eval.board from sparkfun:
http://www.sparkfun.com/commerce/produc ... cts_id=281
what are the conditions for the correct start of program?
DTR Hi (or Low), ON/OFF pin low or High? enable script with AT commands?
What do loader from byteworks?
http://www.thebyteworks.com/gpsgatePy/gpsgatePy.html
Only load scripts or enable script too?
Please for more info if possible!
By byteworks
#58088
GpsgatePy loader uploads the files, enables the startup script, disables SSC bus, enables CMUX (for debug), and enables automatically script startup after 10 seconds. So, after power on, if no AT command is sent on AT commands interface in 10 seconds, the GpsgatePy application starts - there is no need to worry about DTR line (or another one).