- Wed Jun 04, 2008 7:35 pm
#49651
Hi all,
I'm currently doing a university project which is using Gm862-GPS as my main hardware. I had finish and downloaded the SMS and GPRS script into the module and it works fine. Now I need to do a slightly improvement on my project which is include it with geo-fence setting. Geo-fence means when the vehicle is entering or leaving a certain area a msg will send to the server to inform that particular vehicle has entering to leaving the geo-fence zone. I have the idea is comparing the Geo-fence zone coordinates with the current vehicle coordinates,if it was the same then a signal will to send to the server through GPRS. Anyone here can help me with the python code?How to write the python code to get this feature? Helps are highly appreciated. Thanks.
I'm currently doing a university project which is using Gm862-GPS as my main hardware. I had finish and downloaded the SMS and GPRS script into the module and it works fine. Now I need to do a slightly improvement on my project which is include it with geo-fence setting. Geo-fence means when the vehicle is entering or leaving a certain area a msg will send to the server to inform that particular vehicle has entering to leaving the geo-fence zone. I have the idea is comparing the Geo-fence zone coordinates with the current vehicle coordinates,if it was the same then a signal will to send to the server through GPRS. Anyone here can help me with the python code?How to write the python code to get this feature? Helps are highly appreciated. Thanks.