- Sun Sep 03, 2023 6:42 am
#243517
Hello all,
I'm trying to run a simple Bluetooth test on a custom Artemis board:
How should I fix this?
I'm trying to run a simple Bluetooth test on a custom Artemis board:
Code: Select all
My PC recognizes the module (with the name "test") but when trying to connect I get the following error:
#include <ArduinoBLE.h>
BLEService customService("19B10000-E8F2-537E-4F6C-D104768A1214"); // Define a custom service UUID
BLEStringCharacteristic customCharacteristic("19B10001-E8F2-537E-4F6C-D104768A1214", BLERead | BLEWrite, 100); // Use a default UUID
void setup() {
// Start BLE
BLE.begin();
// Set a local name for the device
BLE.setLocalName("test");
// Add the service and characteristic
customService.addCharacteristic(customCharacteristic);
BLE.addService(customService);
// Start advertising
BLE.advertise();
Serial.begin(9600);
}
void loop() {
// Your Arduino code logic goes here
// Read the value from the characteristic
BLEDevice central = BLE.central();
if (central) {
if (customCharacteristic.written()) {
Serial.println("Received: " + customCharacteristic.value());
}
}
}
Code: Select all
In Serial output AES failed... retrying: 0
How should I fix this?