- Thu Jan 12, 2023 3:22 pm
#238291
Hello,
For a long time I had no success getting my 320x240 Sharp Memory Display (which I have connected to my Redboard Artemis ATP) to work well. With the Adafruit GFX library, it worked just fine (albeit very slowly) with bit-banged spi, but it did not work with HW spi, using the MbedSPI class as in the included Example06_SPI.
What is perhaps unusual about this display is that it expects LSB first bit order. I was eventually able to make it work by hacking the gfx lib to reverse the bits of each byte before transmitting (0b10100011 -> 0b11000101). What I find curious is that once I had it working, changing the definition of SPI_ORDER has no effect, it keeps working. So I believe this is the cause of my problems - the SPI transfer does not seem to care about the SPI_ORDER setting, and always transmits each byte in order of most significant bit to least significant bit.
Below is a minimal-ish program (based on the SPI example, using no external libraries) that successfully drives my display (showing "static") over hw SPI whether SPI_ORDER is set to LSBFIRST or MSBFIRST - I would expect this setting to make a difference? Or do I need to set it in some other way?
Thank you,
Andreas
For a long time I had no success getting my 320x240 Sharp Memory Display (which I have connected to my Redboard Artemis ATP) to work well. With the Adafruit GFX library, it worked just fine (albeit very slowly) with bit-banged spi, but it did not work with HW spi, using the MbedSPI class as in the included Example06_SPI.
What is perhaps unusual about this display is that it expects LSB first bit order. I was eventually able to make it work by hacking the gfx lib to reverse the bits of each byte before transmitting (0b10100011 -> 0b11000101). What I find curious is that once I had it working, changing the definition of SPI_ORDER has no effect, it keeps working. So I believe this is the cause of my problems - the SPI transfer does not seem to care about the SPI_ORDER setting, and always transmits each byte in order of most significant bit to least significant bit.
Below is a minimal-ish program (based on the SPI example, using no external libraries) that successfully drives my display (showing "static") over hw SPI whether SPI_ORDER is set to LSBFIRST or MSBFIRST - I would expect this setting to make a difference? Or do I need to set it in some other way?
Thank you,
Andreas
Code: Select all
#include <SPI.h>
#define SHARP_SCK SPI_CLK
#define SHARP_MOSI SPI_SDO
#define SHARP_MISO NC
#define SHARP_CS D13
#define SHARP_VDD D12
#define SPI_FREQ 2000000
#define SPI_MODE SPI_MODE0
#define SPI_ORDER LSBFIRST
MbedSPI mySPI(NC, SHARP_MOSI, SHARP_SCK); // declare the custom MbedSPI object mySPI
extern "C" SPIName spi_get_peripheral_name(PinName mosi, PinName miso, PinName sclk);
void setup() {
Serial.begin(115200);
while (!Serial) {}
Serial.printf("Using SPI %d\n", spi_get_peripheral_name(SHARP_MOSI, SHARP_MISO, SHARP_SCK));
Serial.printf("SPI_ORDER is %d\n", SPI_ORDER);
pinMode(SHARP_CS, OUTPUT);
digitalWrite(SHARP_CS, LOW);
pinMode(SHARP_VDD, OUTPUT);
digitalWrite(SHARP_VDD, HIGH);
mySPI.begin();
}
const size_t len = 44;
uint8_t tx_buff[len];
uint8_t swap(uint8_t b) {
b = (b & 0xF0) >> 4 | (b & 0x0F) << 4;
b = (b & 0xCC) >> 2 | (b & 0x33) << 2;
b = (b & 0xAA) >> 1 | (b & 0x55) << 1;
return b;
}
int i = 0;
void loop() {
int vcom = i++ % 2;
// fill with random data
for (int j = 0; j < len; j++) {
tx_buff[j] = rand();
}
// except first byte for command
tx_buff[0] = 0x80 | (vcom << 6);
// and last two bytes for trailer
tx_buff[len - 2] = 0x00;
tx_buff[len - 1] = 0x00;
tx_buff[1] = swap(i);
mySPI.beginTransaction(SPISettings(SPI_FREQ, SPI_ORDER, SPI_MODE));
digitalWrite(SHARP_CS, HIGH);
mySPI.transfer(&tx_buff, len);
mySPI.endTransaction();
digitalWrite(SHARP_CS, LOW);
}