- Fri Jun 19, 2020 11:46 am
#216408
I am tinkering with a Redboard Artemis with Sparkfun CAN-bus shield. I have never worked with either of these, so maybe I am doing something wrong. The headers are soldered on and inserted onto the RBA. I have the Sparkfun Redboard Artemis selected in the board manager, and the COM port is correct and selected. I am able to upload example sketches for my RFM69 just fine. So I removed the the RFM69 transceiver to play with the CAN shield which is probably fine as far as hardware connections go. Hopefully the pin mapping isn't a problem as the layout looks the same as an Uno board which the shield was designed for. The problem is in the software hurdle I can't seem to get past to even test the shield.
Has anyone gotten their Artemis boards to work with the SF CAN library? I can't get this stuff to compile at all. First, I would get an error telling me that the include library <util/delay.h> doesn't exist. It has to do with some timer functions I guess, and I tried to edit the CAN library files and comment out any #include delay.h. So now when I try to compile any of the demo sketches, I get a whopper of an error message instead that might mean the Artemis isn't compatible? See a copy snip of the error.
Can anyone make any sense of this wall of text?
Has anyone gotten their Artemis boards to work with the SF CAN library? I can't get this stuff to compile at all. First, I would get an error telling me that the include library <util/delay.h> doesn't exist. It has to do with some timer functions I guess, and I tried to edit the CAN library files and comment out any #include delay.h. So now when I try to compile any of the demo sketches, I get a whopper of an error message instead that might mean the Artemis isn't compatible? See a copy snip of the error.
Can anyone make any sense of this wall of text?
Code: Select all
Arduino: 1.8.13 (Windows Store 1.8.39.0) (Windows 10), Board: "SparkFun RedBoard Artemis, 921600, SparkFun Variable Loader (Recommended)"
WARNING: library SparkFun_CAN-Bus_Arduino_Library-master claims to run on avr architecture(s) and may be incompatible with your current board which runs on apollo3 architecture(s).
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:78,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_gpio.h:69:6: error: conflicting types for 'padMode'
void padMode(uint8_t pad, am_hal_gpio_pincfg_t mode, ap3_err_t *retval);
^~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_gpio.h:68:6: note: previous declaration of 'padMode' was here
void padMode(uint8_t pad, am_hal_gpio_pincfg_t mode);
^~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_gpio.h:72:6: error: conflicting types for 'pinMode'
void pinMode(uint8_t pin, am_hal_gpio_pincfg_t mode);
^~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_gpio.h:71:6: note: previous declaration of 'pinMode' was here
void pinMode(uint8_t pin, uint8_t mode);
^~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_gpio.h:73:6: error: conflicting types for 'pinMode'
void pinMode(uint8_t pin, am_hal_gpio_pincfg_t mode, ap3_err_t *retval);
^~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_gpio.h:71:6: note: previous declaration of 'pinMode' was here
void pinMode(uint8_t pin, uint8_t mode);
^~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_gpio.h:81:79: error: expected ';', ',' or ')' before '=' token
unsigned long pulseIn(uint8_t pinNumber, uint8_t state, unsigned long timeout = 1000000L);
^
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:67,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
c:\users\tai nguyen\documents\arduinodata\packages\sparkfun\tools\arm-none-eabi-gcc\8-2018-q4-major\arm-none-eabi\include\stdlib.h:70:5: error: expected identifier or '(' before 'int'
int abs (int);
^~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino_defines.h:58:21: error: expected ')' before '>' token
#define abs(x) ((x) > 0 ? (x) : -(x))
^
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Print.h:26,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Stream.h:26,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/HardwareSerial.h:27,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:29,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:80,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Printable.h:24:1: error: unknown type name 'class'
class Print;
^~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Printable.h:32:1: error: unknown type name 'class'
class Printable
^~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Printable.h:33:1: error: expected '=', ',', ';', 'asm' or '__attribute__' before '{' token
{
^
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Stream.h:26,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/HardwareSerial.h:27,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:29,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:80,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Print.h:36:1: error: unknown type name 'class'
class Print
^~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Print.h:37:1: error: expected '=', ',', ';', 'asm' or '__attribute__' before '{' token
{
^
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/HardwareSerial.h:27,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:29,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:80,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Stream.h:49:1: error: unknown type name 'class'
class Stream : public Print
^~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Stream.h:49:14: error: expected '=', ',', ';', 'asm' or '__attribute__' before ':' token
class Stream : public Print
^
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:29,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:80,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/HardwareSerial.h:60:1: error: unknown type name 'class'
class HardwareSerial : public Stream
^~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/HardwareSerial.h:60:22: error: expected '=', ',', ';', 'asm' or '__attribute__' before ':' token
class HardwareSerial : public Stream
^
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:80,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:40:20: error: expected '=', ',', ';', 'asm' or '__attribute__' before '<' token
typedef RingBufferN<AP3_UART_RINGBUFF_SIZE> AP3UartRingBuffer;
^
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:58:1: error: unknown type name 'class'
class Uart : public HardwareSerial
^~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:58:12: error: expected '=', ',', ';', 'asm' or '__attribute__' before ':' token
class Uart : public HardwareSerial
^
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:81,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_analog.h:57:11: error: conflicting types for 'servoWrite'
ap3_err_t servoWrite(uint8_t pin, uint32_t val, uint16_t minMicros, uint16_t maxMicros);
^~~~~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_analog.h:56:11: note: previous declaration of 'servoWrite' was here
ap3_err_t servoWrite(uint8_t pin, uint32_t val);
^~~~~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_analog.h:60:11: error: conflicting types for 'tone'
ap3_err_t tone(uint8_t pin, uint32_t freq, uint32_t duration);
^~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_analog.h:59:11: note: previous declaration of 'tone' was here
ap3_err_t tone(uint8_t pin, uint32_t freq);
^~~~
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:84,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/WMath.h:22:13: error: conflicting types for 'random'
extern long random( long ) ;
^~~~~~
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Printable.h:22,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Print.h:26,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Stream.h:26,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/HardwareSerial.h:27,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:29,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:80,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
c:\users\tai nguyen\documents\arduinodata\packages\sparkfun\tools\arm-none-eabi-gcc\8-2018-q4-major\arm-none-eabi\include\stdlib.h:255:6: note: previous declaration of 'random' was here
long random (void);
^~~~~~
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:84,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/WMath.h:23:13: error: conflicting types for 'random'
extern long random( long, long ) ;
^~~~~~
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Printable.h:22,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Print.h:26,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/Stream.h:26,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/HardwareSerial.h:27,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_uart.h:29,
from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:80,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
c:\users\tai nguyen\documents\arduinodata\packages\sparkfun\tools\arm-none-eabi-gcc\8-2018-q4-major\arm-none-eabi\include\stdlib.h:255:6: note: previous declaration of 'random' was here
long random (void);
^~~~~~
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:84,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/WMath.h:28:17: error: conflicting types for 'makeWord'
extern uint16_t makeWord( uint8_t h, uint8_t l ) ;
^~~~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ard_supers/WMath.h:27:17: note: previous declaration of 'makeWord' was here
extern uint16_t makeWord( uint16_t w ) ;
^~~~~~~~
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:87,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1\variants\redboard_artemis/config/variant.h:33:1: error: unknown type name 'class'
class Uart; // Forward declaration of Uart
^~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1\variants\redboard_artemis/config/variant.h:34:13: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'Serial'
extern Uart Serial;
^~~~~~
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1\variants\redboard_artemis/config/variant.h:35:13: error: expected '=', ',', ';', 'asm' or '__attribute__' before 'Serial1'
extern Uart Serial1;
^~~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'spi_putc':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:53:2: error: 'SPDR' undeclared (first use in this function); did you mean 'SDA'?
SPDR = data;
^~~~
SDA
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:53:2: note: each undeclared identifier is reported only once for each function it appears in
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:56:12: error: 'SPSR' undeclared (first use in this function); did you mean 'PSTR'?
while( !( SPSR & (1<<SPIF) ) )
^~~~
PSTR
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:56:23: error: 'SPIF' undeclared (first use in this function); did you mean 'TPI'?
while( !( SPSR & (1<<SPIF) ) )
^~~~
TPI
In file included from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:40:
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_write_register':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:37:19: error: 'PORTB' undeclared (first use in this function); did you mean 'PORT'?
#define _port2(x) PORT ## x
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:24:19: note: in expansion of macro '_port2'
#define PORT(x) _port2(x)
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:28:19: note: in expansion of macro 'PORT'
#define _XRS(x,y) PORT(x) &= ~(1<<y)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:17:19: note: in expansion of macro '_XRS'
#define RESET(x) _XRS(x)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:65:2: note: in expansion of macro 'RESET'
RESET(MCP2515_CS);
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_read_register':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:37:19: error: 'PORTB' undeclared (first use in this function); did you mean 'PORT'?
#define _port2(x) PORT ## x
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:24:19: note: in expansion of macro '_port2'
#define PORT(x) _port2(x)
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:28:19: note: in expansion of macro 'PORT'
#define _XRS(x,y) PORT(x) &= ~(1<<y)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:17:19: note: in expansion of macro '_XRS'
#define RESET(x) _XRS(x)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:79:2: note: in expansion of macro 'RESET'
RESET(MCP2515_CS);
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_bit_modify':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:37:19: error: 'PORTB' undeclared (first use in this function); did you mean 'PORT'?
#define _port2(x) PORT ## x
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:24:19: note: in expansion of macro '_port2'
#define PORT(x) _port2(x)
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:28:19: note: in expansion of macro 'PORT'
#define _XRS(x,y) PORT(x) &= ~(1<<y)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:17:19: note: in expansion of macro '_XRS'
#define RESET(x) _XRS(x)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:94:2: note: in expansion of macro 'RESET'
RESET(MCP2515_CS);
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_read_status':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:37:19: error: 'PORTB' undeclared (first use in this function); did you mean 'PORT'?
#define _port2(x) PORT ## x
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:24:19: note: in expansion of macro '_port2'
#define PORT(x) _port2(x)
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:28:19: note: in expansion of macro 'PORT'
#define _XRS(x,y) PORT(x) &= ~(1<<y)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:17:19: note: in expansion of macro '_XRS'
#define RESET(x) _XRS(x)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:109:2: note: in expansion of macro 'RESET'
RESET(MCP2515_CS);
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_init':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:37:19: error: 'PORTB' undeclared (first use in this function); did you mean 'PORT'?
#define _port2(x) PORT ## x
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:24:19: note: in expansion of macro '_port2'
#define PORT(x) _port2(x)
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:29:18: note: in expansion of macro 'PORT'
#define _XS(x,y) PORT(x) |= (1<<y)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:18:18: note: in expansion of macro '_XS'
#define SET(x) _XS(x)
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:124:2: note: in expansion of macro 'SET'
SET(MCP2515_CS);
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:38:18: error: 'DDRB' undeclared (first use in this function); did you mean 'DDR'?
#define _ddr2(x) DDR ## x
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:25:18: note: in expansion of macro '_ddr2'
#define DDR(x) _ddr2(x)
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:32:19: note: in expansion of macro 'DDR'
#define _XSO(x,y) DDR(x) |= (1<<y)
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:20:23: note: in expansion of macro '_XSO'
#define SET_OUTPUT(x) _XSO(x)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:125:2: note: in expansion of macro 'SET_OUTPUT'
SET_OUTPUT(MCP2515_CS);
^~~~~~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:38:18: error: 'DDRD' undeclared (first use in this function); did you mean 'DDR'?
#define _ddr2(x) DDR ## x
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:25:18: note: in expansion of macro '_ddr2'
#define DDR(x) _ddr2(x)
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:33:19: note: in expansion of macro 'DDR'
#define _XSI(x,y) DDR(x) &= ~(1<<y)
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:21:22: note: in expansion of macro '_XSI'
#define SET_INPUT(x) _XSI(x)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:135:2: note: in expansion of macro 'SET_INPUT'
SET_INPUT(MCP2515_INT);
^~~~~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:37:19: error: 'PORTD' undeclared (first use in this function); did you mean 'PORT'?
#define _port2(x) PORT ## x
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:24:19: note: in expansion of macro '_port2'
#define PORT(x) _port2(x)
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:29:18: note: in expansion of macro 'PORT'
#define _XS(x,y) PORT(x) |= (1<<y)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:18:18: note: in expansion of macro '_XS'
#define SET(x) _XS(x)
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:136:2: note: in expansion of macro 'SET'
SET(MCP2515_INT);
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:139:2: error: 'SPCR' undeclared (first use in this function); did you mean 'SCB'?
SPCR = (1<<SPE)|(1<<MSTR) | (0<<SPR1)|(1<<SPR0);
^~~~
SCB
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:139:13: error: 'SPE' undeclared (first use in this function)
SPCR = (1<<SPE)|(1<<MSTR) | (0<<SPR1)|(1<<SPR0);
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:139:22: error: 'MSTR' undeclared (first use in this function); did you mean 'PSTR'?
SPCR = (1<<SPE)|(1<<MSTR) | (0<<SPR1)|(1<<SPR0);
^~~~
PSTR
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:139:34: error: 'SPR1' undeclared (first use in this function); did you mean 'SJW1'?
SPCR = (1<<SPE)|(1<<MSTR) | (0<<SPR1)|(1<<SPR0);
^~~~
SJW1
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:139:44: error: 'SPR0' undeclared (first use in this function); did you mean 'SJW0'?
SPCR = (1<<SPE)|(1<<MSTR) | (0<<SPR1)|(1<<SPR0);
^~~~
SJW0
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:140:2: error: 'SPSR' undeclared (first use in this function); did you mean 'PSTR'?
SPSR = 0;
^~~~
PSTR
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:149:2: warning: implicit declaration of function '_delay_us'; did you mean 'delay'? [-Wimplicit-function-declaration]
_delay_us(10);
^~~~~~~~~
delay
In file included from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:40:
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_check_message':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:39:18: error: 'PIND' undeclared (first use in this function); did you mean 'PIN'?
#define _pin2(x) PIN ## x
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:26:18: note: in expansion of macro '_pin2'
#define PIN(x) _pin2(x)
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:35:20: note: in expansion of macro 'PIN'
#define _XR(x,y) ((PIN(x) & (1<<y)) != 0)
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:22:20: note: in expansion of macro '_XR'
#define IS_SET(x) _XR(x)
^~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:201:11: note: in expansion of macro 'IS_SET'
return (!IS_SET(MCP2515_INT));
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_get_message':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:226:6: warning: implicit declaration of function 'bit_is_set'; did you mean 'timerisset'? [-Wimplicit-function-declaration]
if (bit_is_set(status,6)) {
^~~~~~~~~~
timerisset
In file included from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:40:
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:37:19: error: 'PORTB' undeclared (first use in this function); did you mean 'PORT'?
#define _port2(x) PORT ## x
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:24:19: note: in expansion of macro '_port2'
#define PORT(x) _port2(x)
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:28:19: note: in expansion of macro 'PORT'
#define _XRS(x,y) PORT(x) &= ~(1<<y)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:17:19: note: in expansion of macro '_XRS'
#define RESET(x) _XRS(x)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:239:2: note: in expansion of macro 'RESET'
RESET(MCP2515_CS);
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_send_message':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:287:6: warning: implicit declaration of function 'bit_is_clear'; did you mean 'bitClear'? [-Wimplicit-function-declaration]
if (bit_is_clear(status, 2)) {
^~~~~~~~~~~~
bitClear
In file included from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:40:
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:37:19: error: 'PORTB' undeclared (first use in this function); did you mean 'PORT'?
#define _port2(x) PORT ## x
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:24:19: note: in expansion of macro '_port2'
#define PORT(x) _port2(x)
^~~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:28:19: note: in expansion of macro 'PORT'
#define _XRS(x,y) PORT(x) &= ~(1<<y)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\global.h:17:19: note: in expansion of macro '_XRS'
#define RESET(x) _XRS(x)
^~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:301:2: note: in expansion of macro 'RESET'
RESET(MCP2515_CS);
^~~~~
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'spi_putc':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:60:1: warning: control reaches end of non-void function [-Wreturn-type]
}
^
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c: In function 'mcp2515_check_message':
C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:202:1: warning: control reaches end of non-void function [-Wreturn-type]
}
^
In file included from C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/Arduino.h:81,
from C:\Users\Tai Nguyen\Documents\Arduino\libraries\SparkFun_CAN-Bus_Arduino_Library-master\src\mcp2515.c:33:
At top level:
C:\Users\Tai Nguyen\Documents\ArduinoData\packages\SparkFun\hardware\apollo3\1.1.1/cores/arduino/ard_sup/ap3_analog.h:37:14: warning: 'g_ADCHandle' defined but not used [-Wunused-variable]
static void *g_ADCHandle;
^~~~~~~~~~~
exit status 1
Error compiling for board SparkFun RedBoard Artemis.
This report would have more information with
"Show verbose output during compilation"
option enabled in File -> Preferences.