SparkFun Forums 

Where electronics enthusiasts find answers.

Topics pertaining to the Arduino Core & software used with the Artemis module and Artemis development boards.
User avatar
By jamessukah
#228939
I have the sparkfun redboard artemnis and I want to upload a bin file unto it using the artemis firmware uploader v2.0 but I keep getting errors. I have used different Baud Rate but still it did not work. I also tried to use the blink.bin file provided in the artemis firmware uploader folder to see if it works. but it also did not work. The error message I got is pasted below. This is on a windows machine.

Phase: Setup
Cleared startup blip
Phase: Bootload
Sending 8784 bytes in 5 frames
Error receiving packet
Unknown error
Sending frame #0, length: 0
Upload failed!


Also I want to be able to use the artemis firmware upload on a linux machine but when I double click the linux exe file provided in the linux folder, nothing happens. How can I upload flash my IMU connected to a linux machine without using the artemis firmware uploader, because it is not work for me.

Thank you in advance. :)