- Thu Jul 22, 2021 5:13 pm
#227431
Hi there,
I'm trying to connect a TMP117 sensor via qwiic and a Myoware muscle sensor via the 3.3V rail to an Artemis Nano. The Myoware is powered on, but the TMP117 is not, even though I can recognize that there's an I2C device connected via a scanner. Is this expected behavior? If so, what's the best way to get around this issue if I only want to use one Arduino board with one power source?
I'm trying to connect a TMP117 sensor via qwiic and a Myoware muscle sensor via the 3.3V rail to an Artemis Nano. The Myoware is powered on, but the TMP117 is not, even though I can recognize that there's an I2C device connected via a scanner. Is this expected behavior? If so, what's the best way to get around this issue if I only want to use one Arduino board with one power source?