SparkFun Forums 

Where electronics enthusiasts find answers.

Topics pertaining to the Arduino Core & software used with the Artemis module and Artemis development boards.
User avatar
By amnth
#227277
I am trying to run examples provided by RadioLib LoRa library as it has built-in supports the Artemis Arduino Core.
However all the examples are failing to initialize the Radio.

I am using RadioLib at version 4.4.2: https://github.com/jgromes/RadioLib
I've loaded the SX126x_Transmit.ino as an example.
Code: Select all
// SX1262 has the following connections:
// NSS pin:   10
// DIO1 pin:  2
// NRST pin:  3
// BUSY pin:  9
SX1262 radio = new Module(10, 2, 3, 9);
Code: Select all
void setup() {
  Serial.begin(9600);

  // initialize SX1262 with default settings
  Serial.print(F("[SX1262] Initializing ... "));
  int state = radio.begin();
  if (state == ERR_NONE) {
    Serial.println(F("success!"));
  } else {
    Serial.print(F("failed, code "));
    Serial.println(state);
    while (true);
  }

  // some modules have an external RF switch
  // controlled via two pins (RX enable, TX enable)
  // to enable automatic control of the switch,
  // call the following method
  // RX enable:   4
  // TX enable:   5
  /*
    radio.setRfSwitchPins(4, 5);
  */
}
The example is failing when radio.begin() is called.
Code: Select all
08:21:28.477 -> [SX1262] Initializing ... failed, code -2
Code: Select all
/*!
  \brief Radio chip was not found during initialization. This can be caused by specifying wrong chip type in the constructor
  (i.e. calling SX1272 constructor for SX1278 chip) or by a fault in your wiring (incorrect slave select pin).
*/
#define ERR_CHIP_NOT_FOUND                            -2
Has anyone attempted to use LoRa RadioLib to do peer-to-peer LoRa transmission?