SparkFun Forums 

Where electronics enthusiasts find answers.

Questions about the BatchPCB service

Moderator: robacarp

#2874
The short answer is no.

These orders are batched onto one panel. Everyone on that panel gets the same type board of course. So if you can find enough friends that want a certain setup, let us know. 100 square inch minimum.

If you have a single design that needs special consideration, and you could use 100 square inches, let us know. We will quote you a panel.

If you need 30,000 square inches, we can quote you large batches as well.

Possible thicknesses:
0.5mm 0.8mm 1.6mm 2.0mm 2.5mm 3.0mm

Available solder mask colors:
Red, Green, Black

Email pcbquestions@sparkfun.com for quotes.
By westfw
#3414
Hmm. I'd really like to see a thinner board as a standard option.
0.062 is pretty thick, ESPECIALLY for the small boards where this
service is particularly attractive.