SparkFun Forums 

Where electronics enthusiasts find answers.

Questions about the BatchPCB service

Moderator: robacarp

By ShreddinPB
#158049
Hey guys, I am trying to get a pcb onto batchpcb and I am getting an error that I cant figure out.
Here is the error file
Code: Select all
unmatched 274X paramblock OFA0B0 - len 6
Macro Name = OC8
Macro Consuming 5,1,8,0,0,1.08239X$1,22.5 [2]
PUSH 1.000000
PUSH 8.000000
PUSH 0.000000
PUSH 0.000000
PUSH 1.082390
FETCH 1
MUL
PUSH 22.500000
PRIM 5
Parse_OK
Beginning GCODE run
Ending GCODE run
Created 371 polygons
Found 0 errors
Partitioning....
Grouping...
Distance testing
MergeCount: 277
tests: 14599
Board boundaries: Rect: [0.162400,0.064700] -> [2.913000,1.577300], w: 2.750600, h: 1.512600
Found 94 groups
lengthdb size 0
DRC space fail: [0x1a0fcd0 0x1a0fd70] 0.005600 - 0.006000
DRC space fail: [0x1a0fd70 0x1a0fcd0] 0.005600 - 0.006000
DRC space fail: [0x1a0fe10 0x1a0feb0] 0.005500 - 0.006000
DRC space fail: [0x1a0feb0 0x1a0fe10] 0.005500 - 0.006000
DRC space fail: [0x1a0feb0 0x1a0ff50] 0.005500 - 0.006000
DRC space fail: [0x1a0ff50 0x1a0feb0] 0.005500 - 0.006000
DRC space fail: [0x1a0ff50 0x1a0fff0] 0.005500 - 0.006000
DRC space fail: [0x1a0fff0 0x1a0ff50] 0.005500 - 0.006000
------------------------------------------------
exit status: 255
DRC put out 33 lines of logging code
the fails I see are:
DRC space fail: [0x1a0fcd0 0x1a0fd70] 0.005600 - 0.006000
DRC space fail: [0x1a0fd70 0x1a0fcd0] 0.005600 - 0.006000
DRC space fail: [0x1a0fe10 0x1a0feb0] 0.005500 - 0.006000
DRC space fail: [0x1a0feb0 0x1a0fe10] 0.005500 - 0.006000
DRC space fail: [0x1a0feb0 0x1a0ff50] 0.005500 - 0.006000
DRC space fail: [0x1a0ff50 0x1a0feb0] 0.005500 - 0.006000
DRC space fail: [0x1a0ff50 0x1a0fff0] 0.005500 - 0.006000
DRC space fail: [0x1a0fff0 0x1a0ff50] 0.005500 - 0.006000

The image they send back, as far as I can tell, has nothing on there to tell me what is wrong
You do not have the required permissions to view the files attached to this post.
User avatar
By Ross Robotics
#158058
One problem is you're using BatchPCB. Go to Itead or OSH Park.

The only thing I see is that little IC. What's the pitch on that IC?
By ShreddinPB
#158059
codlink wrote:One problem is you're using BatchPCB. Go to Itead or OSH Park.

The only thing I see is that little IC. What's the pitch on that IC?
Its a Linear LTC 6820 (MSOP16)
MSOP-16 (4.0 x 3.0 mm body width, 0.5 mm pin pitch)